STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ux_device_class_cdc_acm_read_run not working

I am developing a custom board using STM32H523RET6.It has a USB type C port, and I am trying to send some data from PC to the board through it, and decided to use USB CDC ACM with standalone mode. The code is based on this and this.ux_device_class_cd...

HaYa6174 by Associate III
  • 821 Views
  • 4 replies
  • 0 kudos

Resolved! SPI + DMA using LL Library

Hi, I'm using stm32h7, currently working with SPI + DMA in HAL library, because of HAL overhead I want to move to LL library, where can I get the SPI+DMA using LL library examples, regards, Srinath

Resolved! USB Host MCU Middleware on STM32U545

Hi. I'm having trouble using the old USB Host Middleware to read a USB stick with a STM32U545.I've tried to follow this article, doing my best to adapt it for the host middleware and also using the "FatFs_USBDisk" example project for the F767 Nucleo ...

Resolved! ETH H755 Nucleo Hard Faults

Hi Everyone, I've followed STguide on Ethernet on H755 using RTOShttps://community.st.com/t5/stm32-mcus/how-to-create-a-project-for-stm32h7-with-ethernet-and-lwip-stack/ta-p/49308/page/2/show-comments/trueand a github on ETH on bare metal (my case)ht...

Resolved! STM32H7S3L8 Dual ADC Multichannel + DMA

Hello guys,for my bachelors project I have decided to build an embedded signal monitoring and classification tool, based on the STM32H7S3L8 Nucleo dev board (NUCLEO H7S3L8). I want to use all  14 available channels of the 2 adcs (technically each ADC...

htxy by Associate III
  • 600 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.