STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H5 running NetXDuo with KSZ9567R

Hello. I have two setups: one STM32H5 Nucleo eval board and a custom STM32H5 board. The Nucleo runs with the LAN8742 PHY while the eval board runs with the KSZ9567R switch. Both are configured to use RMII. I'm using the NetXDuo stack for both. The Nu...

ADosa.1 by Associate II
  • 631 Views
  • 2 replies
  • 1 kudos

Resolved! Ethern Config and ping test

Good morning, I've been trying to create a simple program for several days that allows me to ping from my laptop to my Nucle F767ZTI board, but to no avail. I'm using CUBE IDE 1.18. I initially followed a tutorial and was able to do it, but only in d...

SMusc.1 by Senior
  • 618 Views
  • 3 replies
  • 5 kudos

STM32F407 ETH Fatal Bus Error

During stress testing involving repeated startup and shutdown, a fatal error was encountered in the STM32F407 Ethernet (ETH) module.The issue was observed during the startup phase, where a problem occurred in the ETH DMA. The DMASR register indicated...

Jerry邵 by Associate II
  • 525 Views
  • 5 replies
  • 0 kudos

Zephyr Blinky LED example not blinking

Split from Zephyr RTOS on Nucleo-F411RE ? - which has been answered.This is a new question.Hi T_HamdiThank you for your response.I have installed the Zephyr IDE and used the Blinky LED example. The firmware was flashed successfully; however, the LED ...

Kumar123 by Associate III
  • 428 Views
  • 1 replies
  • 1 kudos

Resolved! MATLAB/Simulink XCP protocol via LPUART1

Hi all,I failed to run Nucleo-G431RB board using Simulink "Monitor & Tune" mode via Simulink XCP protocol.I've got the error message at Simulink,"Could not connect to target application: XCP internal error: timeout expired, in response to XCP CONNECT...

JellyFish by Associate II
  • 6573 Views
  • 5 replies
  • 3 kudos

Resolved! LTDC Controller not displaying image

I am currently using the STM32N657 on the NUCLEO-N657X0-Q board to drive an 800x480 pixel display with 24-bit color. The display that I am using is the NHD-7.0-800480EF-ASXV#-T. I’m using the built in LTDC controller on the chip. I do know that the c...

DHOUT19_0-1756245275614.png DHOUT19_1-1756245305699.png DHOUT19_2-1756245348090.png DHOUT19_3-1756245465102.png
DHOUT19 by Associate II
  • 1220 Views
  • 3 replies
  • 2 kudos

Resolved! Support for UCPD with N6 with zephyr

I'm curious how hard of a task would it be to get UCPD working with the STM32N6 with zephyr. I see it's supported with the G0* https://docs.zephyrproject.org/latest/boards/st/stm32g071b_disco/doc/index.html From my understanding the UCPD hardware blo...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.