STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! rt-thread project

I created project in stmcube32mx for h5 microcontroller and it works if I manually replace bl main to bl entryin file startup_stm32h563zitx.s.If this manual replacing is a bug or on purpose?Jan

Jan27 by Associate II
  • 1336 Views
  • 10 replies
  • 3 kudos

Resolved! slow data rate with usb cdc on nucleo-h533

Hi All, I'm building an instrument that needs to stream data to a PC at ~4Mbps. People were claiming nearly twice this with USB CDC so I chose the nucleo-h533 board and started with the Ux_Device_CDC_ACM example. I disconnected the USART code and add...

MScha.8 by Associate II
  • 1225 Views
  • 11 replies
  • 3 kudos

STM32L471 BFB2 and FB_MODE question.

Hello,I'm trying DUAL BOOT on STM32L471 and having a problem with SYSCFG->MEMRMP FB_MODE bit.I modified Dual Boot Bank Swap Boot Loader Example for STM32G4 project to fit my board, and everything goes well when the firmware put from the start of BANK...

LWIP freeRTOS and BSD Sockets

Hi, I have started from a project by Adam Berlinger.I have two UDP sockets, one receiving data max 500 bytes/s one sending data 200 bytes every 5 seconds and one TCPIP sending 4K every 20 ms.Netconn Api I have no problem. With BSD sockets, If I work ...

FMarr.2 by Associate III
  • 743 Views
  • 1 replies
  • 0 kudos

STM32H573I - USB MSC device standalone

Just wanted to see if anyone could point me in the right direction regarding a problem I'm having with implementing a USB device using MSC in standalone mode. The code initialises correctly as far as I can tell but as soon as it gets into the main lo...

loz01 by Associate II
  • 769 Views
  • 4 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.