2025-12-09 9:04 PM - last edited on 2025-12-10 3:05 AM by Andrew Neil
Hi
Is it possible to run Zephyr RTOS on the STM32F411RET6 Nucleo board? If it is possible, how can I set up and use Zephyr RTOS on it? Please suggest the steps.
Solved! Go to Solution.
2025-12-10 2:46 AM - edited 2025-12-10 2:46 AM
hello @Kumar123
Yes, it is possible to run Zephyr RTOS on the STM32F411RET6 Nucleo board. For detailed information on board specifications, supported features, and configuration, you can refer to the official Zephyr documentation here:
Zephyr Board: Nucleo F411RE.
also to get started with Zephyr RTOS on the STM32F411RET6 nucleo board, you can follow the official Getting Started Guide provided by the Zephyr Project:
Getting Started Guide — Zephyr Project Documentation.
2025-12-10 2:46 AM - edited 2025-12-10 2:46 AM
hello @Kumar123
Yes, it is possible to run Zephyr RTOS on the STM32F411RET6 Nucleo board. For detailed information on board specifications, supported features, and configuration, you can refer to the official Zephyr documentation here:
Zephyr Board: Nucleo F411RE.
also to get started with Zephyr RTOS on the STM32F411RET6 nucleo board, you can follow the official Getting Started Guide provided by the Zephyr Project:
Getting Started Guide — Zephyr Project Documentation.
2025-12-29 3:06 AM - edited 2025-12-29 3:31 AM
Follow-on question: Zephyr Blinky LED example not blinking.
@Kumar123 - please keep to one question per thread.
Edited to correct link.
2025-12-29 3:21 AM
Hi Andrew Neil
The above link are not open.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.