2025-11-25 10:03 AM
I'm curious how hard of a task would it be to get UCPD working with the STM32N6 with zephyr.
I see it's supported with the G0
* https://docs.zephyrproject.org/latest/boards/st/stm32g071b_disco/doc/index.html
From my understanding the UCPD hardware block is the same between the two chips?
Solved! Go to Solution.
2025-12-24 12:41 AM
Differences mainly lie in number of peripheral instances and clock/reset bus architecture, not in core functionality. Also, note that, minor silicon revisions and optimizations may exist between these 2 families.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-12-24 12:41 AM
Differences mainly lie in number of peripheral instances and clock/reset bus architecture, not in core functionality. Also, note that, minor silicon revisions and optimizations may exist between these 2 families.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-12-26 12:32 PM
Thanks for the info
I decided not to go down the road of linking the address to the device tree to try it.
Currently Zephyr and USB c is kind of the bare minimum. You can see the github issue list here.
https://github.com/zephyrproject-rtos/zephyr/issues/38371
But it's mostly the bare minimum. To minimum for my needs.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.