STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can anyone explain why any STM32H743 Ethernet reception causes all the Rx buffer descriptors to be closed with DESC3 set to 0x00000000 and the RBU status flag set to indicate no more buffers available?

HiWorking on the STM32H743ZI - Ethernet transmission is working but reception not.As shown below there are 4 rx buffer descriptors set up. Each with the DMA ownership, generate interrupt on completion and buffer 1 valid set in DESC3. DESC0 points to ...

0693W00000KdLUKQA3.png 0693W00000KdLUZQA3.png
hpipon957 by Associate III
  • 8281 Views
  • 10 replies
  • 0 kudos

STM32H743 with USB HS, FUSB2805 not detected

I have a custom board with STM32H743VIT6 connected to an external USB HS PHY, the FUSB2805MLX.I am trying to run a bare minimum example setup in STM32CubeMx. Just including a USB HS connection and the device in USB VCP mode. The pin setup is correct,...

LFjær.1 by Associate
  • 1861 Views
  • 1 replies
  • 0 kudos

USART HAL Compatibility with FreeRTOS

I'm trying to send data over the Virtual COM Port of an STM32H745I dev board to a Termite shell inside a FreeRTOS task. I setup USART 3 to run at the settings matching the documentation's virtual COM Port settings, and call the generated initializati...

0693W00000LvUjYQAV.png
EMurp.1 by Associate II
  • 1862 Views
  • 2 replies
  • 0 kudos

STM32L433 IAP

Hi,I have 2 partitions on the STM32L433cct6 :IAP (to upgrade via USB) : 0x08000000 - 0x0800C000Application : 0x0800C000 - 0x08040000I have a function to jump to the application :/* Jump to user application */ JumpAddress = *(__...

MMerc.1 by Senior
  • 2561 Views
  • 4 replies
  • 0 kudos

STM32L0 ADC two channel polling

Posted on November 06, 2016 at 21:04Hi, I am coding an application for STM32L053R8 using the HAL functions. Right now I need to read continuously two analog values via ADC. Because there is no need of high frequency readings, I want to try doing it ...

STM32L0 - How to set Single-Ended Mode on an ADC Channel on STM32 using the HAL library?

Current settings seem to only produce 0x000 to 0x7FF . The HAL API on the STM32L0 only has 2 Parameters in the ADC ChannelConf Type:typedef struct{ uint32_t Channel;    uint32_t Rank;         }ADC_ChannelConfTypeDef;Which is Clearly missing the : ...

X-CUBE-USB-PD install

Hello. I'm trying to figure out X-CUBE-USB-PD. As I understand it, this is an extension for CubeMX, but I can't figure out how to install this extension. Downloaded the project from the link https://github.com/STMicroelectronics/x-cube-usb-pd . I was...

DalOpez by Associate II
  • 1660 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.