2019-02-19 9:26 PM
Current settings seem to only produce 0x000 to 0x7FF . The HAL API on the STM32L0 only has 2 Parameters in the ADC ChannelConf Type:
typedef struct
{
uint32_t Channel;
uint32_t Rank;
}ADC_ChannelConfTypeDef;
Which is Clearly missing the : sConfig.SingleDiff = ADC_SINGLE_ENDED; feature....
Our current Settings:
static void MX_ADC_Init(void)
{
ADC_ChannelConfTypeDef sConfig;
/**Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
*/
hadc.Instance = ADC1;
hadc.Init.OversamplingMode = DISABLE;
hadc.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV1;
hadc.Init.Resolution = ADC_RESOLUTION_12B;
hadc.Init.SamplingTime = ADC_SAMPLETIME_1CYCLE_5;
hadc.Init.ScanConvMode = ENABLED;
hadc.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc.Init.ContinuousConvMode = ENABLED;
hadc.Init.DiscontinuousConvMode = DISABLE;
hadc.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc.Init.DMAContinuousRequests = DISABLE;
hadc.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
hadc.Init.Overrun = ADC_OVR_DATA_PRESERVED;
hadc.Init.LowPowerAutoWait = ENABLE; // new..
hadc.Init.LowPowerFrequencyMode = DISABLE;
hadc.Init.LowPowerAutoPowerOff = DISABLE;
if (HAL_ADC_Init(&hadc) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
// Had hoped THIS would work - but no
if (HAL_ADCEx_Calibration_Start(&hadc, ADC_SINGLE_ENDED) != HAL_OK) {
Error_Handler();
}
// Configure for the selected ADC regular channel to be converted.
sConfig.Rank = 1;
sConfig.Channel = ADC_CHANNEL_8;
if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
/**Configure for the selected ADC regular channel to be converted.
*/
sConfig.Rank = 2;
sConfig.Channel = ADC_CHANNEL_9;
if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
}
Anyone have some thoughts on this? Would REALLY like to get to 0x000 to 0xFFF
2019-02-25 1:33 PM
Anyone??
2022-03-21 2:26 PM
Hi @Community member - could you solve the problem? I would higly appreciate a solution or advice to your problem since I have the same issue.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.