2022-03-21 7:46 AM
Hello. I'm trying to figure out X-CUBE-USB-PD. As I understand it, this is an extension for CubeMX, but I can't figure out how to install this extension. Downloaded the project from the link https://github.com/STMicroelectronics/x-cube-usb-pd . I was given the task to implement the functionality of the project from the example on the stm32f4 device. Please help me figure it out. For the second week I can't figure it out.
2022-03-21 8:46 AM
The version on github doesn't seem to be an extension to CubeMX. There's no *.ioc file.
Just get all the files and run directly the IDE project files provided under Projects/ ... / EWARM, MDK-ARM or STM32CubeIDE.
2022-03-21 9:44 AM
I have already done as you advised. CubeIDE discovered the EVAL_FUSB307_DRP project. If you do not make any changes, the project is built without problems. However , if you remove any .c or .h file, errors appear in the project. So far, they have no thoughts on how to use this project to implement power delivery on stm32f4.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.