2022-03-23 5:19 AM
I have a custom board with STM32H743VIT6 connected to an external USB HS PHY, the FUSB2805MLX.
I am trying to run a bare minimum example setup in STM32CubeMx. Just including a USB HS connection and the device in USB VCP mode.
The pin setup is correct, and the external clocks on the PHY are correct (26MHz in, generates 60MHz on CLK line between MCU and PHY).
I can see that the 60Mhz line is shut down after the call to `USBD_Start(&hUsbDeviceHs)`
The data lines are pulled high at the same time.
The relevant pinout is:
```
PA3 -> USB_OTG_HS_ULPI_DO
PA5 -> USB_OTG_HS_ULPI_CK
PB0 -> USB_OTG_HS_ULPI_D1
PB1 -> USB_OTG_HS_ULPI_D2
PB5 -> USB_OTG_HS_ULPI_D7
PB10 -> USB_OTG_HS_ULPI_D3
PB11 -> USB_OTG_HS_ULPI_D4
PB12 -> USB_OTG_HS_ULPI_D5
PB13 -> USB_OTG_HS_ULPI_D6
PC0 -> USB_OTG_HS_ULPI_STP
PC2_C -> USB_OTG_HS_ULPI_DIR
PC3_C -> USB_OTG_HS_ULPI_NXT
```
However, i cannot get this to work.
The code runs without errors and debugging through it doesn't give me any idea of what might be wrong. All functions return with HAL_OK
The computer does not detect the USB device.
`sudo dmesg | grep usb` gives the following output
```
[27482.966148] usb usb3-port7: attempt power cycle
[27483.622018] usb 3-7: new low-speed USB device number 32 using xhci_hcd
[27483.622532] usb 3-7: Device not responding to setup address.
[27483.830337] usb 3-7: Device not responding to setup address.
[27484.041933] usb 3-7: device not accepting address 32, error -71
[27484.173925] usb 3-7: new low-speed USB device number 33 using xhci_hcd
[27484.174414] usb 3-7: Device not responding to setup address.
[27484.382364] usb 3-7: Device not responding to setup address.
[27484.589893] usb 3-7: device not accepting address 33, error -71
[27484.590002] usb usb3-port7: unable to enumerate USB device
[81863.025532] usb 3-3: reset full-speed USB device number 3 using xhci_hcd
[82185.873876] usb 3-3: reset full-speed USB device number 3 using xhci_hcd
[82306.336339] usb 3-3: reset full-speed USB device number 3 using xhci_hcd
[82758.471075] usb 3-3: reset full-speed USB device number 3 using xhci_hcd
```
It's the same using the USB_DEVICE Middleware in Mass Storace Class mode.
Are there any tricks to getting ULPI USB HS to work on this MCU?
2022-03-23 1:00 PM
Does the host really see the low-speed response or nothing at all.?
Get a physical USB bus analyzer (and somebody who knows how to use it)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.