STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H745I-DISCO UART communication problem

Hello everyone, First of all I am kinda new in ARM (I never use), I am working on the STM32H745I-DISCO board (using the CM7 core) and I am facing a persistent issue with UART . No matter what I try, the RX Interrupt never triggers, and the code never...

EnesUNLU by Associate II
  • 1164 Views
  • 17 replies
  • 5 kudos

STM32L475RCT6 Flash Erase Error

I'll explain Flash Erase Error to the stm32l475rct6 MCU that I'm currently using. Page : 127, Address : 0x0803F800, Bank : FLASH_BANK_1 is defined, and if you try to modify the value after first saving the value in the Flash area, the values already ...

Resolved! STM32H7RS SWR-Bit wont clear; LWIP + FreeRTOS

Hello fellow readers,##Disclaimer##I am using a Nucleo Board, the Nucleo H7S3L8, and HAL_ERROR ist laughing me since 2 days in my face# I think you, dear reader, have heard about the SWR-Bit, which vanishes out as soon the software has restarted succ...

Vidar by Associate III
  • 415 Views
  • 3 replies
  • 1 kudos

netXDuo TCP Server problem

Hello all. I'm writing an application with the NUCLEO-H563ZI board (with the intention to use later the STM32H563 into a custom board). My application will communicate with a master PC via the embedded Ethernet, exchanging process data and commands. ...

Resolved! i2c Error 4

Hi there !i work with DS2482 I2c to one wire . After i send the command reset i need the read the status register until i find one bit at 1, so i wrote my routine in this way  static uint8_t DS2482_Status_Register(void) { uint8_t register_status=0; ...

SGian.1 by Senior
  • 533 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.