STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

For UCPDx controller, I want to configure a sink for 15V/3A(45W) use STM32G0B1RCT6. What's the meaning of UCPD number for 'GP' version LQFP64 package?

Hello, I find there are a note for 'GP' version LQFP64 package.In blank of UCPD, which has the number "1" .The note is: One port with only one CC Line available(supporting limited number of use cases).Is that mean only one UCPD controller( UCPD1 or U...

0693W00000HnkY0QAJ.png
Lmatt.11 by Associate III
  • 1301 Views
  • 1 replies
  • 0 kudos

Disable VBUS_VS_DISCH pin on STUSB4500

We use the STUSB4500 in our design to negotiate with the Host the correct current. In our design we have no connection on the VBUS_VS_DISCH pin. Because of this issue, the PD-Chip does not start negotiation. Is there any way to disable the VBUS_VS_DI...

FMüll.1 by Associate
  • 1391 Views
  • 1 replies
  • 1 kudos

Usbx Azure rtos not working

Hello,I am working on Nucleo-h745ziq board. I initialize the azure-rtos h7 package, enable the Usbx and thread parameter .According the project that given in cubemx of Ux_Device__CDC_ACM accordingly I initialize the parameter only difference is that ...

MDeva.1 by Associate II
  • 6478 Views
  • 6 replies
  • 0 kudos

Bug STM32F429ZI ETH PTP Receive Timestamp

STM32Cube FW_F4 V1.27.1HAL ETH PTPfilestm32f4xx_hal_eth.cfunction HAL_StatusTypeDef HAL_ETH_ReadData(ETH_HandleTypeDef *heth, void **pAppBuff)line 1115, 1117   /* Get timestamp high */   heth->RxDescList.TimeStamp.TimeStampHigh = dmarxdesc->DESC6;   ...

vekli by Associate II
  • 2381 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.