STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! File System to store HTML Web pages in NUCLEO-H745-ZIQ

I am trying to develop simple HTTP Web Server using NUCLEO-H745-ZIQ board.The idea is to have file system to store our HTML web pages.Do you have an example code to achieve this ? Or else please suggest us a way to have file system to load our html ...

PB S.1 by Associate II
  • 3985 Views
  • 7 replies
  • 0 kudos

how to connect MQTTS with STM32F411 and W5500.

Hello,I am trying to make MQTTS connection by W5500 chip. I am using STM32F411 and generating code with STM32CubeMX and compiling with Makefile. I’m unable to find any sample code that works for this, Please share if anyone have any idea how can i ma...

AGaut.4 by Associate
  • 2046 Views
  • 0 replies
  • 0 kudos

Resolved! Error in sending email from STM32H7 based processor board using SMTP client APIs in LWIP TCP/IP stack.

Hi, I am trying to create an SMTP client application using LWIP to send/receive emails from my STM32H7 based processor board, I am using smtp_send_mail() to send emails, although this functions returns ERR_OK, i couldn't monitor the emails being sent...

Nagaraj1 by Associate II
  • 1615 Views
  • 1 replies
  • 0 kudos

Have two USB Audio Device Class

I have a STM32F446 MCU. I want to use the two USB ports featured by the MCU and have a single Audio Device Class on each USB but once one is selected in the CubeMX, the other is greyed out.

TLest.2 by Associate II
  • 3725 Views
  • 6 replies
  • 0 kudos

Creating multiple HID devices on STM32 controller

I recently got into STM32. My goal is to use my 1 controller to simulate multiple keyboard on my Windows computer.Currently, I managed to get a setup that works for 1 keyboard (1 HID device) using the Custom HID device settings on the CubeIDE. I'm tr...

pgold.1 by Associate
  • 2459 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.