STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F746-DISCOVERY. USB HOST FS MSC not working. Application state never go to state "APPLICATION READY"

Hello,I am working on a project with an STM32F746BGT6. I am supposed to read a binary file on an USB key. I have a code with USB OTG-FS working on STM32F4, but not with a F7. The variable "Appli_state" is never changed to "APPLICATION_READY" which un...

GNico.2 by Associate II
  • 5086 Views
  • 5 replies
  • 0 kudos

hi everybody i tried on stm32f407VG board using dp83848 PHY in RMii mode to connect to LAN network via ethernet cable but still failed so any solution i am using lwip like middleware .

salut tout le monde j'ai essayé sur la carte stm32f407VG en utilisant dp83848 PHY en mode RMii pour me connecter au réseau LAN via un câble ethernet mais j'ai quand même échoué, donc toute solution que j'utilise lwip comme middleware.

Mhrag.1 by Associate II
  • 2680 Views
  • 5 replies
  • 0 kudos

What component should I use to give access to the Internet to an stm32 nucleo f303ze board in places without Wi-fi?

Hi, I'm sorry if this is the wrong place to ask.I've got several Nucleo F303ze boards collecting data in several locations and I want them to send said data to my web page to process it. To grant them internet access I would usually use a wi-fi modul...

JMarc.5 by Associate II
  • 989 Views
  • 0 replies
  • 0 kudos

How is it possible to modify “tracex_custom.trxc�? to customize TraceX User Events when Azure RTOS TraceX installed through Microsoft Store?

Description:In ThreadX, it is possible to create custom TraceX User Events with: tx_trace_user_event_insert()This feature is explained in this artice: Chapter 10 - Customer user events…here: https://learn.microsoft.com/en-us/azure/rtos/tracex/chapter...

SS13 by Associate II
  • 1089 Views
  • 0 replies
  • 0 kudos

Query on class b for STM32U585 Controller

Hello Support Team,Have a wonderful day.We are selected Trustzone MCU STM32U585ZIT6Q for our product we have some queries regarding the certification Based on the attached user guide snapshot, we could understand this U5 series chip have a Class B li...

_legacyfs_online_stmicro_images_0693W00000bkRDMQA2.png

Resolved! Hello, Is there an example for the STM32H7 ETH HAL V11.0 (new reworked ETH driver) without the LWIP. All the example i found are coupled with the LWIP. Thanks.

Following function are tied to the LWIP functions and i do not want to use any LWIP etc...How to bypass that ?void HAL_ETH_RxAllocateCallback(uint8_t **buff) { struct pbuf_custom *p = LWIP_MEMPOOL_ALLOC(RX_POOL); if (p) { /* Get the buff fr...

FB__1 by Associate III
  • 2993 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.