2023-05-27 9:30 AM
I recently got into STM32.
My goal is to use my 1 controller to simulate multiple keyboard on my Windows computer.
Currently, I managed to get a setup that works for 1 keyboard (1 HID device) using the Custom HID device settings on the CubeIDE.
I'm trying to progress into having multiple keyboards (multiple HID devices) and I'm having a really hard time figuring out what to do.
From what Iv'e read on the forums, I understand that there are 2 option for what I'm trying to do:
Composite USB
Having multiple HID interfaces on the same USB output.
I'm mostly trying to do the second option, but I think either one would work for me.
I'm really struggling with instruction on what to do, I found a few forum posts, but I couldn't really understand what to actually do, I don't really understand what I actually need to change in my code in order to have multiple HID interfaces in it.
If anyone could give me some tips or resources it would be highly appreciated, thanks
2023-05-31 6:00 AM
Hello @pgold.1 and welcome to the Community :) ,
To implement the USB device composite, I recommend you to start from an available example.
For that I recommend you to take a look to this HID composite application (Mouse + Keyboard) application based on USBX middleware running on STM32H747.
So, try to get inspired from the instructions in the readme file.
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.