STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32G0B1 USB device not recognized in Windows 10

Hello,I'm using STM32G0B1-Nucleo (with no USB user connector), and I am trying to program USB device (I tried virtual COM, HID and MSC separately).I'm using the STM32CubeMx with STM32CubeG0 FW V1.5.1 to generate the configuration with PA12 and PA11 f...

0693W00000NsGxsQAF.png 0693W00000NsGxxQAF.png
Houssem by Associate II
  • 11024 Views
  • 10 replies
  • 0 kudos

I know sounds dumb, but how do you configure SysTick

I need to run SysTick every microseconds instead of every millisecond. So I called: SysTick_Config(SystemCoreClock / 1000000);except that delay never ended, because the interrupt was low priority so: HAL_InitTick(TICK_INT_PRIORITY);Except this s...

RobG by Associate III
  • 24952 Views
  • 9 replies
  • 3 kudos

Small Floating point values

Hi,I have a general question regarding the problem I am facing.Currently, the pSpeed Value is very small (for example 3.4E-7) and when I perform a square for such values it becomes smaller. When I pass the Square data value to the arm_sqrt_f32() func...

ZHaid1_0-1702573772577.png
ZHaid.1 by Associate II
  • 3147 Views
  • 4 replies
  • 0 kudos

USB Host Bulk Input NAK || STM32U575

Hi All,I am working on the STM32U575 for host mass storage class.I am not using stm32 middle ware for this due to some reasons.I am using TinyUSB open-source stack to implement the Host mass storage class.with my current implementation I am able to u...

RRajb.2 by Associate III
  • 13786 Views
  • 19 replies
  • 4 kudos

How to disable the USB cable detection?

Hello, I am using a STM32G473RC microcontroller and want to use usart3 to update the firmware.I also use the CAN-BUS on pin PA11 and PA12. These pins (PA11, PA12) are also USB pins (DP and DM).When I start the bootloader (BOOT = 1 + RESET), the "USB ...

GHese.1 by Associate II
  • 7907 Views
  • 8 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.