STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Immediate !!!

  Hi, I am using a STM32F429 board and I have compiled u boot and freeRTOS for this board's core. I wanna run a FreeRTOS on this board on U boot. My compilation processes  was successfull. But when I wanna run this on u boot. I am loading FreeRTOS .b...

mus4 by Associate
  • 1872 Views
  • 3 replies
  • 0 kudos

STM32WB55RGV6 in mode DFU no update firmware

Hello. I'm a beginner with the STM32WB55RGV6, but I have a lot of experience with other microcontrollers from different manufacturers. I bought a STM32WB55RGV6 NUCLEO development board to load the Flipper Zero firmware onto it. However, I'm facing ma...

zurczurc by Associate
  • 2610 Views
  • 1 replies
  • 0 kudos

Resolved! STM32L0x1 svd

Hi,I have STM32L0x1 svd v1.3, and it seems the PWR_CR LPSDSR bit is missing.Is there a more recent svd file? I can't seem to find it.Thanks

Resolved! STM UART DMA to receive Multibyte packet

hi, This is question regarding UART reception.UART configured with 115200 8 N1 I have a project where i need to receive a multibyte packet on UART and the length is not fixed.My Queries 1> Which approach should I take to receive a multibyte packet.2>...

STM32H7 HAL SPI too slow for my application

I'm using HAL SPI drivers to read some MCP23S17 expander chips. I am sending a 2 byte command and receiving a 6 byte response. The trouble is there is 6 mS of delay between the write and read. Code:  // read encoder expander chips for encoder button ...

STM32 does not reset after DFU by USB

Posted on November 17, 2017 at 20:27I have already read several posts about the subject. including 'DFU: LEAVE does not jump to application'.and 'Reset after firmware upgrade'Context : STM32F072RBusing either DfuSeCommand.exe or DfuSeDemoUsing the D...

Problems with i2s

Hello, I am doing a project wich takes audio from an ESP32 via I2S, process it and then send bia i2S to an amplifier wich manage I2S signals as input.HARD:ESP32 (source of audio)ST nucleo F401Re (processing unit)Amp: MAX98357A.I manage to make work p...

guidoglorioso01_0-1702841431168.png guidoglorioso01_1-1702841444427.png guidoglorioso01_2-1702841454891.png

STM32U5A5 Semp put/get speed test

I have callback ISR code (from UART) where I put in Semaphore put and other code with Threadx static implementation with stack (SRAM2), Semaphore get, etc. I placed two GPIO signals to measure the timing between put and get. I set the compiler to opt...

Riscy by Senior
  • 957 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.