STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32U5 ADC VREFINT_CAL_ADDR

The #define value for VREFINT_CAL_ADDR in the stm32u5xx_ll_adc.h HAL file has an odd value address (0x0BFA 07A5). This causes attempts to access the value to fault with an unaligned access. I have checked for other devices (STM32F4, STM32L0, Etc.) an...

cpegeo by Associate
  • 2594 Views
  • 2 replies
  • 0 kudos

Driver issue Windows 11

Dear Community,I keep getting an error message when installing the latest STM32 virtual com port driver on both Windows 10 and Windows 11 - can anybody suggest a solution?Thanks,Sascha

0693W00000WKkwiQAD.png 0693W00000WKkwxQAD.png
SSchu.12 by Associate
  • 19236 Views
  • 3 replies
  • 0 kudos

Experience with Upwork, Fiverr, etc.

I just read a post where @pavel suggested using Upwork or Fiverr to get some programming work done.  These sites might be a big help to me if I can get a programming job done by someone else without a lot of overhead on my part. I'd appreciated any c...

magene by Senior II
  • 1856 Views
  • 3 replies
  • 1 kudos

Resolved! IRQ Handlers with LL drivers

I generally prefer the STM Low Level drives and chose that driver family for most peripheral in CubeMX Project Manager->Advanced Settings->Driver Selector.  There seem to be one disadvantage: the IRQHandlers are not generated as weak which I think ha...

magene by Senior II
  • 3258 Views
  • 3 replies
  • 0 kudos

WPA-Enterprise on STWINBX1

I'm trying to connect to a WPA-Enterprise network (EAP-TLS) with the STWINBX1 board. And in this context, I have several questions aboutabout using the mx_wifi driver.I'm basing my project on the Nx_WebServer and Nx_MQTT_Client examples from the STM3...

chhhhak by Associate II
  • 1006 Views
  • 0 replies
  • 0 kudos

STM32H5 USBX hub class

Hi,a new STM32H5 based design (Azure RTOS) needs two USB host ports. We want to use a hub.To give this a try I modified UX_Host_DualClass example from STM32H573I-DK /STM32Cube_FW_H5_V1.1.0 to run on my NUCLEO-STM32H563ZI board. I removed all the USBP...

MFuch.3 by Associate II
  • 3371 Views
  • 2 replies
  • 1 kudos

Resolved! STM32H5 timer triggered SPI won't trigger

I have a new (to me) STM32H563 Nucleo board and I just need a bit of help with the new style DMA system. I haven't been able to find any reasonable examples for the H5 or U5 that have the new DMA controller, so I'm asking for help here.The end goal i...

Resolved! Problem using 'NUCLEO-G0B1RE' with USB Host CDC class

I'm trying to communicate with an external device with a USB-C Device interface in CDC Serial class.I'm following the steps as shown in the videohttps://www.youtube.com/watch?v=V3sMN-ErKPw&list=PLnMKNibPkDnFFRBVD206EfnnHhQZI4Hxa&index=20However, in m...

hgalindo by Associate II
  • 5332 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.