2022-09-29 12:42 AM
Hello,
I'm working with a STM32F767, on a custom pcb and a Nucleo-144, same behavior, so it's probably not hardware / board related.
Source code:
Problem:
I played with the lwIP timers and the TCP retransmission timers, that reduced the delay to these 400 ms, before that it was sometimes 1.5 s.
I turned of everything in source code that might block.
I changed all ETH transfers to zero copy, TX with interrupt for non-blocking PTPd.
Any ideas?
Edit: I uploaded the most important source code parts - the complete zero copy (mostly non-Cube/HAL) ethernetif.c / .h
Edit 2: I uploaded the updated source, having removed some blunders...
For now TCP is running smoothly with 25.6 Mbps
Solved! Go to Solution.
2022-10-01 6:20 AM
At least I found the cause of the late collision error:
It's the HAL / Cube setting up of the LAN8742, rather the reading of the PHY settings.
I used the "old" STM32F7 Cubae HAL stuff for setting this up - the last part remaining where I use HAL / Cube for ethernet...
It's reading back the wrong PHY register, and then sets its own duplex mode wrongly in MACCR.
Aaaaaarrrghhh....!
I found that because www told me that the most probable cause for the late collision error is that one side has the wrong duplex mode set.
Then I found that someone in another forum complained about the wrong register reading in HAL / Cube for LAN8742.
Here's the wrong and corrected version from stm32f7xx_hal_eth.c :
I hope that and the code above might help other people.
#define PHY_REGNEW_SSR (uint16_t)31 /* PHY Special Status Register */
#define PHY_REGNEW_SSR_SPD_100M ((uint32_t)1 << 3) /* Speed Indication, bits 4:2 */
#define PHY_REGNEW_SSR_DUPL_FULL ((uint32_t)1 << 4) /* Speed Indication, bits 4:2 */
#if( 0 )
/* 2022-10-01
* HAL reading back wrong register for status of LAN8742!
*/
/* WRONG */
/* Read the result of the auto-negotiation */
if((HAL_ETH_ReadPHYRegister(heth, PHY_SR, &phyreg)) != HAL_OK)
{
/* In case of write timeout */
err = ETH_ERROR;
/* Config MAC and DMA */
ETH_MACDMAConfig(heth, err);
/* Set the ETH peripheral state to READY */
heth->State = HAL_ETH_STATE_READY;
/* Return HAL_ERROR */
return HAL_ERROR;
}
/* Configure the MAC with the Duplex Mode fixed by the auto-negotiation process */
if((phyreg & PHY_DUPLEX_STATUS) != (uint32_t)RESET)
{
/* Set Ethernet duplex mode to Full-duplex following the auto-negotiation */
(heth->Init).DuplexMode = ETH_MODE_FULLDUPLEX;
}
else
{
/* Set Ethernet duplex mode to Half-duplex following the auto-negotiation */
(heth->Init).DuplexMode = ETH_MODE_HALFDUPLEX;
}
/* Configure the MAC with the speed fixed by the auto-negotiation process */
if((phyreg & PHY_SPEED_STATUS) == PHY_SPEED_STATUS)
{
/* Set Ethernet speed to 10M following the auto-negotiation */
(heth->Init).Speed = ETH_SPEED_10M;
}
else
{
/* Set Ethernet speed to 100M following the auto-negotiation */
(heth->Init).Speed = ETH_SPEED_100M;
}
#else
/* CORRECT */
/* Read the result of the auto-negotiation */
if( HAL_ETH_ReadPHYRegister(heth, PHY_REGNEW_SSR, &phyreg) != HAL_OK )
{
/* In case of write timeout */
err = ETH_ERROR;
/* Config MAC and DMA */
ETH_MACDMAConfig(heth, err);
/* Set the ETH peripheral state to READY */
heth->State = HAL_ETH_STATE_READY;
/* Return HAL_ERROR */
return HAL_ERROR;
}
/* Configure the MAC with the Duplex Mode fixed by the auto-negotiation process */
if( phyreg & PHY_REGNEW_SSR_DUPL_FULL )
{
/* Set Ethernet duplex mode to Full-duplex following the auto-negotiation */
(heth->Init).DuplexMode = ETH_MODE_FULLDUPLEX;
}
else
{
/* Set Ethernet duplex mode to Half-duplex following the auto-negotiation */
(heth->Init).DuplexMode = ETH_MODE_HALFDUPLEX;
}
/* Configure the MAC with the speed fixed by the auto-negotiation process */
if( phyreg & PHY_REGNEW_SSR_SPD_100M )
{
/* Set Ethernet speed to 100M following the auto-negotiation */
(heth->Init).Speed = ETH_SPEED_100M;
}
else
{
/* Set Ethernet speed to 10M following the auto-negotiation */
(heth->Init).Speed = ETH_SPEED_10M;
}
#endif
2022-09-29 3:22 AM
Just added the most important source code parts ...
With "killing my application" I just mean that data transfer from SAI to ETH is stopped, because RAM is not big enough for such a time gap.
When I stop SAI DMA and restart ETH TX, it works again for a few seconds.
Further observations:
2022-09-29 5:54 AM
So, tcp_output() somehow doesn't work on the unsent queues.
I put some error messages in tcp_output() / tcp_output_segment(), nothing.
I checked the lwIP mem stats, all below maximum.
I read back the PHY registers, 100M full duplex.
The problem right now is, that I have the feeling that I have looked everywhere...
2022-09-30 4:26 AM
Not everywhere:
I just started checking TX descriptor 0 = status for errors:
packets get lost / TX aborted because of late collision error.
Okay, at least I know why the packet's gone...
But that still doesn't explain this long retransmission delay.
2022-10-01 6:20 AM
At least I found the cause of the late collision error:
It's the HAL / Cube setting up of the LAN8742, rather the reading of the PHY settings.
I used the "old" STM32F7 Cubae HAL stuff for setting this up - the last part remaining where I use HAL / Cube for ethernet...
It's reading back the wrong PHY register, and then sets its own duplex mode wrongly in MACCR.
Aaaaaarrrghhh....!
I found that because www told me that the most probable cause for the late collision error is that one side has the wrong duplex mode set.
Then I found that someone in another forum complained about the wrong register reading in HAL / Cube for LAN8742.
Here's the wrong and corrected version from stm32f7xx_hal_eth.c :
I hope that and the code above might help other people.
#define PHY_REGNEW_SSR (uint16_t)31 /* PHY Special Status Register */
#define PHY_REGNEW_SSR_SPD_100M ((uint32_t)1 << 3) /* Speed Indication, bits 4:2 */
#define PHY_REGNEW_SSR_DUPL_FULL ((uint32_t)1 << 4) /* Speed Indication, bits 4:2 */
#if( 0 )
/* 2022-10-01
* HAL reading back wrong register for status of LAN8742!
*/
/* WRONG */
/* Read the result of the auto-negotiation */
if((HAL_ETH_ReadPHYRegister(heth, PHY_SR, &phyreg)) != HAL_OK)
{
/* In case of write timeout */
err = ETH_ERROR;
/* Config MAC and DMA */
ETH_MACDMAConfig(heth, err);
/* Set the ETH peripheral state to READY */
heth->State = HAL_ETH_STATE_READY;
/* Return HAL_ERROR */
return HAL_ERROR;
}
/* Configure the MAC with the Duplex Mode fixed by the auto-negotiation process */
if((phyreg & PHY_DUPLEX_STATUS) != (uint32_t)RESET)
{
/* Set Ethernet duplex mode to Full-duplex following the auto-negotiation */
(heth->Init).DuplexMode = ETH_MODE_FULLDUPLEX;
}
else
{
/* Set Ethernet duplex mode to Half-duplex following the auto-negotiation */
(heth->Init).DuplexMode = ETH_MODE_HALFDUPLEX;
}
/* Configure the MAC with the speed fixed by the auto-negotiation process */
if((phyreg & PHY_SPEED_STATUS) == PHY_SPEED_STATUS)
{
/* Set Ethernet speed to 10M following the auto-negotiation */
(heth->Init).Speed = ETH_SPEED_10M;
}
else
{
/* Set Ethernet speed to 100M following the auto-negotiation */
(heth->Init).Speed = ETH_SPEED_100M;
}
#else
/* CORRECT */
/* Read the result of the auto-negotiation */
if( HAL_ETH_ReadPHYRegister(heth, PHY_REGNEW_SSR, &phyreg) != HAL_OK )
{
/* In case of write timeout */
err = ETH_ERROR;
/* Config MAC and DMA */
ETH_MACDMAConfig(heth, err);
/* Set the ETH peripheral state to READY */
heth->State = HAL_ETH_STATE_READY;
/* Return HAL_ERROR */
return HAL_ERROR;
}
/* Configure the MAC with the Duplex Mode fixed by the auto-negotiation process */
if( phyreg & PHY_REGNEW_SSR_DUPL_FULL )
{
/* Set Ethernet duplex mode to Full-duplex following the auto-negotiation */
(heth->Init).DuplexMode = ETH_MODE_FULLDUPLEX;
}
else
{
/* Set Ethernet duplex mode to Half-duplex following the auto-negotiation */
(heth->Init).DuplexMode = ETH_MODE_HALFDUPLEX;
}
/* Configure the MAC with the speed fixed by the auto-negotiation process */
if( phyreg & PHY_REGNEW_SSR_SPD_100M )
{
/* Set Ethernet speed to 100M following the auto-negotiation */
(heth->Init).Speed = ETH_SPEED_100M;
}
else
{
/* Set Ethernet speed to 10M following the auto-negotiation */
(heth->Init).Speed = ETH_SPEED_10M;
}
#endif
2022-10-01 6:20 AM
The problem with lwIP's super late retransmission remains...
2022-10-10 11:05 PM
The problem with lwIP's super late retransmission still remains...
But it's not that urgent anymore, because now I haven't seen a retranmission for some days.
I have uploaded some updated source code for those who are interested in zero-copy ethernet IO for STM32F7 without OS, and mostly without HAL.
I stole it myself from everywhere and mixed it up... :D
2023-10-20 5:52 AM
Hi LCE,
I'm trying to use LwIP with zero-copy Tx on STM32H7. Did you succeded to do it? Do you have code example ?
For now when I use zero-copy Tx, I have an issue on my implementation of low_level_output where I don't have enough DMA decriptor available.
2023-12-17 10:18 PM
Hi,
i reduced the time for retransmission in tcp_priv.h:
#ifndef TCP_TMR_INTERVAL
#define TCP_TMR_INTERVAL 25//usermodify:before it was 250 /* The TCP timer interval in milliseconds. */
#endif /* TCP_TMR_INTERVAL */
I use STM32H725IGK6 + PHY ADIN1100. Code generated by CUBEMX. No RTOS, with ETH and with LWIP.
Another time improvement was to disable nagle algorithm (to force sending short messages):
#define tcp_nagle_disable(pcb) tcp_set_flags(pcb, TF_NODELAY)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.