STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Stm32f429

Hi allI'm want to send a string from one stm32 to another stm32 to blink an led on it I'm using uart polling method to do that.The communication happens and led blinks only if I press the Reset button once I switch off and on power supply. What shoul...

harry123 by Senior II
  • 5595 Views
  • 13 replies
  • 5 kudos

HAL Ethernet API

Hello. I want to use raw ethernet with HAL API. Is there any example for it ? I dont want to use LWIP, just raw ethernet frames and communicate between 2 board. Any example for guide could help me alot

HAL_Delay function does not return

I have a bare metal board with an STM32H723ZGT6.I can connect and program the device.Initially I tried to use the HAL_Delay function but I found it hung the program never returning.This I determined by illuminating an LED on each side of the function...

MDeac.1 by Associate III
  • 6074 Views
  • 8 replies
  • 6 kudos

Dual port ethernet

Hey,I use STM32H745, I created ETH communication on the M4 core and it works well.Now I want ETH communication with two ports, one port per core.It is possible?In each core before the main while, I do:MX_LWIP_Init();/* create new tcp pcb */tcpb = tcp...

ACohe.3 by Associate II
  • 5369 Views
  • 7 replies
  • 1 kudos

Tick OS to Tick LSE Conversion

HiThis is a general question regarding entering sleep, so whatever part you know and can explain will benefit greatly.The questions are much around the function LpTimerStart, which in general converts OS ticks to LSE clock ticks. The number 1e12 ( or...

DS.4 by Senior II
  • 1309 Views
  • 1 replies
  • 1 kudos

Resolved! ADC in dual regular simultaneous mode - no DMA result

Hi, I'm using ADC1 and ADC2 of a STM32F303RE in dual regular simultaneous mode. Each ADC should sample 5 independent channels and a sampling cycle is triggered by software, so I don't use continuous mode.I do get DMA interrupts and everything seems t...

NRumm1_0-1706385188133.png NRumm1_1-1706385325073.png NRumm1_2-1706385372075.png
NRumm.1 by Associate III
  • 2862 Views
  • 1 replies
  • 0 kudos

Resolved! RTC Alarm on STM32F401RCT6

Hello, I've been using the RTC lately and it works correctly except for one thing, the alarm. Below you can see the function HAL generatedstatic void MX_RTC_Init(void) { /* USER CODE BEGIN RTC_Init 0 */ /* USER CODE END RTC_Init 0 */ RTC_Tim...

Hesseltjuuh_0-1698702547947.png Hesseltjuuh_1-1698702558649.png Hesseltjuuh_2-1698702596937.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.