STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! About USBD_HID_SendReport

The value returned from USBD_HID_SendReport always returns USBD_FAIL,What settings are wrong? We think we am doing the settings in project.ioc correctly.[IDE]STM32CubeIDE 1.14.0Connectivity -> USB_OTG_FS -> [Mode]Device_OnlyMiddleware -> USB_DEVICE -...

Decompression of SD card Files

Hi,I am using STM32H5 microcontroller with Free-RTOS environment.Interfaced SD card with the MCU using LittleFS file system.My SD card has Compressed files, I wanted to decompress them and write to the separate folder. Is there any libraries supporte...

PB S.1 by Associate II
  • 3240 Views
  • 6 replies
  • 0 kudos

Resolved! STM32G0B1 USART3 DMA receiving whole data and set it to application layer for process on FreeRTOS?

Dear SIR,I am trying to STM32G0B1 USART3 DMA receiving data from PC and do processing on MCU.I add code in callback function HAL_UARTEx_RxEventCallback()these code are try to get the whole package ending with '\r' and set a flag to notice the FreeRTO...

EJohn_0-1706420440960.png
E-John by Associate III
  • 2310 Views
  • 2 replies
  • 0 kudos

Resolved! Can't see COM port in STM-CUBE monitor UCPD software

Hello,I trying to follow the steps provided in this video : https://www.youtube.com/watch?v=Z_Sn6CBbz-kFollowed each step, compiled, and successfully uploaded the firmware.I am able to see the COM port COM34 in my device manager as shown in attached ...

DGehl.1 by Associate
  • 7202 Views
  • 5 replies
  • 1 kudos

DWT and Microsecond Delay

Hello everyoneI want to use dwt unit to create microsecand delay function. How safe is it to use the DWT unit ? Does it only work in debug mode or does it also work in runtime ?Is there a guarentee that every time the MCU is reset it will start up pr...

burakatc by Associate II
  • 9631 Views
  • 6 replies
  • 3 kudos

Resolved! STM32F7 PTP Support

Hello!,I got a custom PCB with a STM32F76 MCU with a PHY chip.Running Freetos CMSIS V1, and LwIP. I want to setup the MCU as a PTP slave/client. Is there a way to configure this in the .ioc file?Looking through the drivers enabled HAL_ETH_USE_PTP in ...

stevof12 by Associate
  • 4031 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.