STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FreeRTOS acquisition and release?

Hello Everyone,I have a Problem with to acquisition DATA  from One TASK to another and release data.And there is another problem that I can not access  Data from One task to another task.how to use and when can we use , in this code i have to use acq...

NetXDuo custom phy interface

HelloI have STM32H563 with KSZ8081 ethernet phy. On FreeRTOS + LWIP i was able to define the PHY in CubeMX and it was basically working out of the box. However on the NetXDuo when i select Custom Phy Interface I am a bit lost. Are there any guideline...

Resolved! stm32f4 CAN protocol implementation

Hi,i am new to HAL Libraries. i am learning to work with CAN BUS using HAL Libraries. Can any one please post an example of STM32F CAN BUS using HAL Libraries. I searched about the existing examples but their isn't any example with new firmware. im n...

_kalpesh by Associate III
  • 4457 Views
  • 4 replies
  • 1 kudos

stm32f7508-dk board not working

  after writing below flash related code in stm32f7508-dk board , controller is not working display getting blank and , it is also not detecting . can any one help me hot to erase the code and reload the my code void SetupFlashMemory(){//setup memory...

kishor by Associate II
  • 3282 Views
  • 2 replies
  • 0 kudos

Reading input at high frequency

Hi,I've encountered a problem with digital input probing. I have two signals connected to my GPIO on the STM32 F411; the first one is the CMD line, and the second is CLK. Based on the CLK, I would like to read incoming bits on CMD, but only for a spe...

tjak by Associate II
  • 4276 Views
  • 9 replies
  • 7 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.