STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! NetxDuo not working with a static IP addresss

 Hello everyone,  I'm getting my feet wet with ThreadX and NetxDuo.I'm using a NUCLEO-H563ZI board.I started by building and flashing the Nx_UDP_Echo_Server example project to the board using the STM32CubeIDE.This worked right away. The board got add...

Systick IRQ priority and HAL_Delay()

Hello everyone,return to the issue of problems that can arise using the HAL_Delay (), within the Interrupt service functions in projects for embedded systems without RTOS.Briefly: the HAL_Delay (), uses the interrupts thrown every mSec by the system ...

0693W00000UnkBcQAJ.jpg
LVara.1 by Associate II
  • 3386 Views
  • 3 replies
  • 0 kudos

STM32F769I DSI SingleBuffer example with custom timing

Hello!I am working to use the STM32F769I + LCD_DSI_VideoMode_SingleBuffer code example with a different timing output. I was able to get both the 720x480 and 720x576 resolution examples working with no issue. I added a 720p resolution and also got th...

TB7 by Associate
  • 1619 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H753ZI adc oversample CUBEmx error

Hello all,I bought two NUCLEO-H753ZI to experiment the ADC.Used the CUBEMX inside the STM32CubeIDE to configure the ADC to do 4x oversample (ADC1 Oversampling Ratio = "Oversampling ratio 4x").Then generated the code, but it does not compile: ... hadc...

linuxfan by Associate II
  • 1470 Views
  • 1 replies
  • 0 kudos

erase and write internal flash

Do I need to disable global interrupts for internal flash erase and write operations?  __disable_irq(); erase(); __enable_irq(); __disable_irq(); write(); __enable_irq();      

Resolved! STM32F4 EtherNet/IP library

I'm looking to use an STM32F407I for EtherNet/IP communication with some industrial motors and sensors.I cannot seem to find a library that would help me do that for the STM32F4.I found this, but I didn't really understand how to use the solution tha...

unkn0wn by Associate II
  • 5994 Views
  • 6 replies
  • 2 kudos

Resolved! LSM303DLHC STM32F411E

Hello everyone,  I am working with the STM32F411E and i am trying to make the LSM303DLHC working on my board. At this moment i am using this lib: https://github.com/STMicroelectronics/STM32CubeL4/blob/master/Drivers/BSP/Components/lsm303dlhc/lsm303dl...

ThienNguyen0301_1-1712166978775.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.