STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

PHY ETH implementation

Hi, community!As I am dealing with STM32 at the first time, I need help. With my colleague we are doing our first project on STM32 (stm32F767ZITx). We need TCP/IP, so I've added to project FreeRTOS-PLUS. According to FreeRTOS-Plus-TCP Networking Tuto...

braboar by Associate
  • 1235 Views
  • 1 replies
  • 0 kudos

Resolved! Differnce between UART and RS232

Hello everyone, I'am designing a model rocket flight computer. This is a two stage rocket so that's mean I will use two flight computer.Flight computers should have a communication between themselfs. For this communication which one is better? Direct...

testbenchmark_0-1716662112256.png

Resolved! Is the ITTIA database free for the STM32?

Hi CommunityI'm working on a project with stm32F407VET6, and I need a database for storing data. I found the ITTIA DB, and I install it from stm32 cube ide in the middleware categories (FreeRTOS support) but when I read the documentation in the offic...

Resolved! STM32U575 VREFBUF Driver bug when 2.5V is set

Hello,Just fount a bug on the LL driver of VREFBUF on STM32U575when you want to configure internal Vref to 2.5V and you use the nest function:LL_VREFBUF_SetVoltageScaling(LL_VREFBUF_VOLTAGE_SCALE3);where LL_VREFBUF_VOLTAGE_SCALE3  should set VRS bits...

Daniel_A by Associate
  • 1668 Views
  • 1 replies
  • 2 kudos

Resolved! Image reading from uSD card vs USD pen drive

Hi,I have to read both image files(BMP and JPEG) and also text files from either uSD or USB pen drive. But - despite having written quite a bit of code through the years - I have never developed any code that does that specifically. nor do I have pre...

Ricko by Senior III
  • 3674 Views
  • 7 replies
  • 4 kudos

FATFS f_mount problem

Hi,I am trying to program on keil based on sdio with STM32H753ZI MCU.I am able to successfully initialize the sdcard FATFS_LinkDriver(&SD_Driver, SDPath),and I use HAL_SD_Erase() to erase ,itˊs successful ,but when i use f_mount() function it stuck i...

Joseph5241_1-1716369138524.png Joseph5241_2-1716369634059.png

STM32F407 discovery board: USB and I2C issue

Is there anyone who experience this issue? I use eeprom with I2C and USB OTG communication in STM32F407 discovery board. There is no common GPIO pin. whenever I use USB OTG to write something in eeprom through I2C, USB and I2C looks disabled in same ...

Jimmy_LEE by Associate II
  • 3060 Views
  • 6 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.