2024-04-16 10:58 PM
after writing below flash related code in stm32f7508-dk board , controller is not working
display getting blank and , it is also not detecting . can any one help me hot to erase the code and reload the my code
void SetupFlashMemory(){
//setup memory
// Modify Flash Address according to target MCU
HAL_FLASH_Unlock();
FLASH_Erase_Sector(11, FLASH_VOLTAGE_RANGE_4);
HAL_FLASH_Lock();
}
//write to memory
void FlashWrite()
{
HAL_FLASH_Unlock();
for(uint32_t x = 0; x < 30; x++)
{
HAL_FLASH_Program( FLASH_TYPEPROGRAM_WORD, flashAddress, ((uint8_t *)wrBuf)[x]);
flashAddress++;
}
HAL_FLASH_Lock();
}
//read
void FlashRead(){
flashAddress = 0x080E0000 ; // 0x0800F400; // 0x90000000
for(uint32_t k=0; k<5; k++)
{
*((uint8_t *)rdBuf + k) = *(uint8_t *)flashAddress;
flashAddress++;
}
}
2024-05-23 9:52 AM
Hello @kishor,
To erase the code on the stm32f7508-dk card, have you tried using the STM32Cube programmer?
Please do not hesitate to provide any necessary information so that I can help you more effectively.
Thanks and best regards,
Dorsaf
2024-05-23 10:03 AM
Use "Connect Under Reset" options
Use BOOT0 = HIGH to stop your code running, either via a switch, jumper, or tack soldering where necessary.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.