STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-CELLULAR: how to work with STM32H7 (M7) ?

Hi, friends.I am making X-CUBE-CELLULAR working on STM32H750 MCU.my hardware with follow function:USART1 for print DEBUGUSART2 for LTE CELLUAR (with lwip)ETH RMII enabled (with freertos_plus_tcp)QSPI enabledI am building amazon FreeRTOS worked on my ...

saico by Associate II
  • 2186 Views
  • 3 replies
  • 0 kudos

Resolved! I2C detect repeated start condition

Hi!I'm creating an i2c-slave using a stm32g0-series. There are two types of messages that need to be supported, a write-then-read, and a write-only.The write-then-read starts with a write-message of a register address of the slave device (1 byte). Th...

sigmuha by Associate II
  • 3089 Views
  • 4 replies
  • 2 kudos

STM32U545 I2C HAL weirdness

Hi.I'm working on a project using I2C on the U545, and I've noticed that all the HAL_I2C_Slave_* functions include the following:/* Enable Address Acknowledge */hi2c->Instance->CR2 &= ~I2C_CR2_NACK;However, the STM32U5 Reference manual states that wr...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.