STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H753: Receiving Messages via UART

I'm working with an STM32H753 MCU and trying to receive messages from a PC via UART to implement a simple state machine. The idea is that the MCU should switch to different states based on the received message.Initially, I attempted to use fgets(mess...

doronzzz by Associate II
  • 3002 Views
  • 8 replies
  • 4 kudos

Strange Output in I2C

I am using STM32F103C8T6 and developed on STM32CubeIDE. This equipment has  six similar  I2C boards (same ICs, same function)  connected to the master which are addressed accordingly. Each of these boards have 8 digital Inputs amounting to 8 bit valu...

CK.3 by Associate III
  • 1290 Views
  • 2 replies
  • 1 kudos

Unable to communicate with SPI bootloader

Hi,​I am trying to use the ROM bootloader on the STM32G071 to change the contents of specific flash sections. I was able to enter the bootloader just fine, at least I think so because I can see in the debugger how different points in the address spac...

FLewz.1 by Associate III
  • 2011 Views
  • 3 replies
  • 0 kudos

Use Internal OPAMP as Inverting AMP

Hii, I have a query regarding internal op amp , i.e. how we use internal op amp as a inverting amp. , what are the process to initialize the internal op amp in cubemx (HAL driver) and the output is shared to the adc pin.

Harsh_18 by Associate III
  • 851 Views
  • 0 replies
  • 0 kudos

1 PPS (GPS) STM32F429

Hello,I want to develop a firmware to synchronize an Ocxo on a 1PPS GPS reference signal. I have a Nucleo card with a stm32f429 to do the first tests. The configuration: 1 1PPS input (1 second), 1 10Mhz input reference of the OCXO, 1 DAC output, the ...

PSEBA.1 by Associate II
  • 1399 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.