2021-08-22 11:06 PM
Hi, friends.
I am making X-CUBE-CELLULAR working on STM32H750 MCU.
my hardware with follow function:
USART1 for print DEBUG
USART2 for LTE CELLUAR (with lwip)
ETH RMII enabled (with freertos_plus_tcp)
QSPI enabled
I am building amazon FreeRTOS worked on my board,
when using RMII ETH everything work fine,
but when change to LTE CELLUAR, something BAD.
Andy body can help me.
2021-08-22 11:06 PM
==============================DEBUG msg for RMII ETH======================================
13 4083 [iot_thread] [INFO ][DEMO][4081] ---------STARTING DEMO---------
14 4085 [iot_thread] [INFO ][INIT][4085] SDK successfully initialized.
15 4085 [iot_thread] [INFO ][DEMO][4085] Successfully initialized the demo. Network type for the demo: 4
16 4085 [iot_thread] [INFO] Creating a TLS connection to xxxxxxxxxxx.ats.iot.cn-north-1.amazonaws.com.cn:8883.
17 4088 [EMAC-task] Heap: current 145176 lowest 145128
18 4144 [iot_thread] DNS[0xB152]: The answer to 'xxxxxxxxxxx.ats.iot.cn-north-1.amazonaws.com.cn' (52.80.68.38) will be stored
19 4144 [iot_thread] DNS[0xB152]: The answer to 'xxxxxxxxxxx.ats.iot.cn-north-1.amazonaws.com.cn' (52.80.33.106) will be stored
20 4434 [EMAC-task] Heap: current 122184 lowest 122184
21 4517 [EMAC-task] Network buffers: 54 lowest 54
22 5403 [EMAC-task] RX descriptors 7/8
23 6755 [EMAC-task] Heap: current 109720 lowest 107272
24 8337 [EMAC-task] Heap: current 96368 lowest 96368
25 10305 [iot_thread] [DEBUG] Encoded size for length 24 is 1 bytes.
26 10306 [iot_thread] [DEBUG] CONNECT packet remaining length=24 and packet size=26.
27 10306 [iot_thread] [DEBUG] CONNECT packet size is 26 and remaining length is 24.
28 10306 [iot_thread] [DEBUG] Encoded size for length 24 is 1 bytes.
29 10306 [iot_thread] [DEBUG] Length of serialized CONNECT packet is 26.
30 10308 [iot_thread] [DEBUG] BytesSent=26, BytesRemaining=0
31 10308 [iot_thread] [DEBUG] Successfully sent packet at time 6223.
32 10308 [iot_thread] [DEBUG] Sent 26 bytes of CONNECT packet.
33 10309 [iot_thread] [DEBUG] No data was received from the transport.
34 10310 [iot_thread] [DEBUG] No data was received from the transport.
35 10311 [iot_thread] [DEBUG] No data was received from the transport.
36 10312 [iot_thread] [DEBUG] No data was received from the transport.
37 10322 [iot_thread] [DEBUG] No data was received from the transport.
38 10323 [iot_thread] [DEBUG] No data was received from the transport.
39 10324 [iot_thread] [DEBUG] No data was received from the transport.
40 10325 [iot_thread] [DEBUG] No data was received from the transport.
41 10326 [iot_thread] [DEBUG] No data was received from the transport.
47 10340 [iot_thread] [DEBUG] No data was received from the transport.
54 10349 [iot_thread] [DEBUG] No data was received from the transport.
59 10364 [iot_thread] [DEBUG] No data was received from the transport.
66 10380 [iot_thread] [DEBUG] No data was received from the transport.
72 10386 [iot_thread] [DEBUG] No data was received from the transport.
77 10401 [iot_thread] [DEBUG] No data was received from the transport.
83 10416 [iot_thread] [DEBUG] No data was received from the transport.
90 10423 [iot_thread] [DEBUG] No data was received from the transport.
96 10439 [iot_thread] [DEBUG] No data was received from the transport.
105 10603 [SubPub0] [INFO] Sending subscribe request to agent for topic filter: xniot/work/340351303335 with id 1
106 10622 [MQTT Agent] [DEBUG] Encoded size for length 28 is 1 bytes.
107 10622 [MQTT Agent] [DEBUG] Subscription packet remaining length=28 and packet size=30.
108 10622 [MQTT Agent] [DEBUG] SUBSCRIBE packet size is 30 and remaining length is 28.
109 10622 [MQTT Agent] [DEBUG] Encoded size for length 28 is 1 bytes.
110 10622 [MQTT Agent] [DEBUG] Length of serialized SUBSCRIBE packet is 30.
111 10626 [MQTT Agent] [DEBUG] BytesSent=30, BytesRemaining=0
112 10626 [MQTT Agent] [DEBUG] Successfully sent packet at time 6541.
113 10626 [MQTT Agent] [DEBUG] Sent 30 bytes of SUBSCRIBE packet.
114 10636 [MQTT Agent] [DEBUG] No data was received from the transport.
115 11636 [MQTT Agent] [DEBUG] Encoded size for length 3 is 1 bytes.
116 11638 [MQTT Agent] [DEBUG] BytesReceived=3, BytesRemaining=0, TotalBytesReceived=3.
117 11638 [MQTT Agent] [INFO] Packet received. ReceivedBytes=3.
118 11638 [MQTT Agent] [DEBUG] Received packet of type 90.
119 11638 [MQTT Agent] [DEBUG] Packet identifier 1.
120 11638 [MQTT Agent] [DEBUG] Topic filter 0 accepted, max QoS 0.
121 11638 [MQTT Agent] [DEBUG] Returned Command Context 0 to pool
122 11639 [MQTT Agent] [DEBUG] No data was received from the transport.
123 11729 [SubPub0] [INFO] Received subscribe ack for topic xniot/work/340351303335 containing ID 1
124 11747 [SubPub0] [INFO] {"TotalCNT": 1,"ErrorCNT": 0,"Localid": 0,"TaskNumber": 0}
125 11766 [MQTT Agent] [INFO] Publishing message to xniot/dtos/340351303335.
126 11766 [MQTT Agent] [DEBUG] Encoded size for length 107 is 1 bytes.
127 11766 [MQTT Agent] [DEBUG] Encoded size for length 107 is 1 bytes.
128 11766 [MQTT Agent] [DEBUG] PUBLISH packet remaining length=107 and packet size=109.
129 11766 [MQTT Agent] [DEBUG] PUBLISH packet size is 109 and remaining length is 107.
130 11766 [MQTT Agent] [DEBUG] Encoded size for length 107 is 1 bytes.
131 11766 [MQTT Agent] [DEBUG] Serialized PUBLISH header size is 27.
132 11779 [MQTT Agent] [DEBUG] BytesSent=27, BytesRemaining=0
133 11779 [MQTT Agent] [DEBUG] Successfully sent packet at time 7694.
134 11779 [MQTT Agent] [DEBUG] Sent 27 bytes of PUBLISH header.
135 11782 [MQTT Agent] [DEBUG] BytesSent=82, BytesRemaining=0
136 11782 [MQTT Agent] [DEBUG] Successfully sent packet at time 7697.
137 11782 [MQTT Agent] [DEBUG] Sent 82 bytes of PUBLISH payload.
138 11782 [MQTT Agent] [DEBUG] Returned Command Context 1 to pool
139 11783 [MQTT Agent] [DEBUG] No data was received from the transport.
140 11962 [SubPub0] [INFO] Task 0 waiting for publish 0 to complete.
141 11968 [SubPub0] [INFO] Publish 0 completed successfully.
142 11983 [SubPub0] [INFO] Short delay before next publish...
143 12784 [MQTT Agent] [DEBUG] No data was received from the transport.
144 13793 [MQTT Agent] [DEBUG] No data was received from the transport.
145 14795 [MQTT Agent] [DEBUG] No data was received from the transport.
146 15805 [MQTT Agent] [DEBUG] No data was received from the transport.
147 16806 [MQTT Agent] [DEBUG] No data was received from the transport.
148 17807 [MQTT Agent] [DEBUG] No data was received from the transport.
2021-08-22 11:07 PM
==============================DEBUG msg for CELLULAR======================================
9 25734 [iot_thread] [INFO ][DEMO][25734] ---------STARTING DEMO---------
10 25736 [iot_thread] [INFO ][INIT][25736] SDK successfully initialized.
11 25736 [iot_thread] [INFO ][DEMO][25736] Successfully initialized the demo. Network type for the demo: 4
12 25736 [iot_thread] [INFO] Creating a TLS connection to xxxxxxxxxxx.ats.iot.cn-north-1.amazonaws.com.cn:8883.
13 32151 [iot_thread] [DEBUG] Encoded size for length 24 is 1 bytes.
14 32151 [iot_thread] [DEBUG] CONNECT packet remaining length=24 and packet size=26.
15 32151 [iot_thread] [DEBUG] CONNECT packet size is 26 and remaining length is 24.
16 32151 [iot_thread] [DEBUG] Encoded size for length 24 is 1 bytes.
17 32151 [iot_thread] [DEBUG] Length of serialized CONNECT packet is 26.
18 32167 [iot_thread] [DEBUG] BytesSent=26, BytesRemaining=0
19 32167 [iot_thread] [DEBUG] Successfully sent packet at time 6431.
20 32167 [iot_thread] [DEBUG] Sent 26 bytes of CONNECT packet.
21 32267 [iot_thread] [DEBUG] Encoded size for length 2 is 1 bytes.
22 32267 [iot_thread] [DEBUG] BytesReceived=2, BytesRemaining=0, TotalBytesReceived=2.
23 32267 [iot_thread] [INFO] Packet received. ReceivedBytes=2.
24 32267 [iot_thread] [INFO] CONNACK session present bit not set.
25 32267 [iot_thread] [INFO] Connection accepted.
26 32267 [iot_thread] [INFO] Received MQTT CONNACK successfully from broker.
27 32269 [iot_thread] [INFO] MQTT connection established with the broker.
28 32269 [iot_thread] [INFO] Session present: 0
29 32359 [SubPub0] [INFO] Sending subscribe request to agent for topic filter: xniot/work/340351303335 with id 1
30 32378 [MQTT Agent] [DEBUG] Encoded size for length 28 is 1 bytes.
31 32378 [MQTT Agent] [DEBUG] Subscription packet remaining length=28 and packet size=30.
32 32378 [MQTT Agent] [DEBUG] SUBSCRIBE packet size is 30 and remaining length is 28.
33 32380 [MQTT Agent] [DEBUG] Encoded size for length 28 is 1 bytes.
34 32380 [MQTT Agent] [DEBUG] Length of serialized SUBSCRIBE packet is 30.
35 32393 [MQTT Agent] [DEBUG] BytesSent=30, BytesRemaining=0
36 32393 [MQTT Agent] [DEBUG] Successfully sent packet at time 6657.
37 32395 [MQTT Agent] [DEBUG] Sent 30 bytes of SUBSCRIBE packet.
38 32535 [MQTT Agent] [DEBUG] Encoded size for length 3 is 1 bytes.
39 32535 [MQTT Agent] [DEBUG] BytesReceived=3, BytesRemaining=0, TotalBytesReceived=3.
40 32535 [MQTT Agent] [INFO] Packet received. ReceivedBytes=3.
41 32535 [MQTT Agent] [DEBUG] Received packet of type 90.
42 32535 [MQTT Agent] [DEBUG] Packet identifier 1.
43 32535 [MQTT Agent] [DEBUG] Topic filter 0 accepted, max QoS 0.
44 32537 [MQTT Agent] [DEBUG] Returned Command Context 0 to pool
45 32612 [SubPub0] [INFO] Received subscribe ack for topic xniot/work/340351303335 containing ID 1
46 32630 [SubPub0] [INFO] {"TotalCNT": 1,"ErrorCNT": 0,"Localid": 0,"TaskNumber": 0}
47 32648 [SubPub0] [INFO] Task 0 waiting for publish 0 to complete.
48 42664 [SubPub0] [INFO] Short delay before next publish...
49 52672 [SubPub0] [INFO] {"TotalCNT": 2,"ErrorCNT": 1,"Localid": 1,"TaskNumber": 0}
50 52690 [SubPub0] [INFO] Task 0 waiting for publish 1 to complete.
2025-03-06 11:54 PM
Hi saico,
have you founf a solution at the end?
Im also struggling with X-CUBE-CELLULAR
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.