STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! which file starts STM32

I do have this demo program in which main.c is disabled so it would start from main_pinpong.c which is the only file withint main( void ){included in target build startup_stm32l476xx.s is supposed to be the startup file but I do not see any reference...

Untitled.png
MNapi by Senior III
  • 2469 Views
  • 5 replies
  • 4 kudos

Resolved! Timer based using thread X

Hi!!I am using ThreadX to develop a project.As far as I know, when using FreeRTOS, it is highly recommended to switch from SysTick to another timer.Is it the same for ThreadX?Therefore, I am using TIM7, which is a simple timer. I was wondering where ...

Can't ping IPv6 in stm32f769I discovery

I am using LWIP 2.1.2 in stm32f769I discovery board.I can ping IPv4 from my PC.But i can't ping IPv6.I have enabled the Autoconfig(Stateless).As per my understanding the IP address will be created based on the MAC.My MAC is 00:80:e1:00:00:00Link loca...

KP.1132 by Associate II
  • 1477 Views
  • 1 replies
  • 1 kudos

HAL_ADC_PollForConversion gets stuck

I'm writing software that involves reading a single ADC value from my STM32H7R3V8H6, however it is getting stuck in HAL_ADC_PollForConversion(&hadc1, HAL_MAX_DELAY);.If i switch the delay to a smaller value it runs through but it still returns a time...

dfshea by Associate III
  • 7610 Views
  • 17 replies
  • 1 kudos

Resolved! Differentiating multiple CDC-ACM's

I have implemented a dual CDC-ACM USBX device, and would like to incorporate a mechanism to programmatically differentiate the two ACM's at the Host.  One mechanism would be to have each ACM carry with it it's own Serial Number, but I am at a loss as...

Resolved! Enter and exit standby mode using single button

Hello,   I am using STM32L073RBT6 controller. I want to use standby mode in my battery operated instrument. I want to use single tactile button to enter and exit standby mode. Is it possible to do??  What if I allocate another nearby pin as GPIO inte...

JeetS by Associate II
  • 1199 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.