STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! FreeRTOS vs ThreadX for STM32U575

Hi!I want to build a project for STM32U575. I want to use FreeRTOS, but it seems like there are some functions that won't work with it (like the SD). Is there any place where I can see what works or doesn't with each one? Or if  I can use FreeRTOS an...

ire by Associate II
  • 2688 Views
  • 6 replies
  • 0 kudos

Cannot Connect to STM32G0B0CET6

Hello, I am trying to flash a STM32G0B0CET6 and keep getting "Error: No STM32 target found!" When trying to connect. Through the power supply I can see that the device properly resets. The voltage target also goes to 0 when the device turns off. I am...

ra345j by Associate
  • 662 Views
  • 3 replies
  • 2 kudos

Resolved! Error creating queues with threadX

Hello,I’m working on an embedded project using ThreadX, and I’ve encountered what appears to be a queue memory overflow issue.I’ve created two queues: one for data messages and one for events. Both are configured to hold 100 messages of the following...

Why use DMA when you've got shared RAM?

I've inherited some code, the original owner is long gone, and I'm trying to understand his code which has ZERO comments (I'm sure I'm not the only person who's been in this position)It's using the STM32H747IGT6 so it's dual core, got one M4 and one ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.