2025-06-03 10:47 AM
Hello,
I am trying to flash a STM32G0B0CET6 and keep getting "Error: No STM32 target found!" When trying to connect.
Through the power supply I can see that the device properly resets. The voltage target also goes to 0 when the device turns off. I am using an ST-Link V2 with a Tag-connect TC2050-ARM2010 and TC2050-IDC cable to program.
2025-06-03 11:45 AM
Has it ever worked?
Does correct voltage get detected by STM32CubeProgrammer?
Consider showing the schematic.
2025-06-04 12:35 AM
Hello @ra345j
Ensure all connections between the ST-Link and the STM32 board are secure, and also check that the jumpers are set correctly. Update the ST-Link firmware using STM32CubeProgrammer if needed. If the issue persists, try the "Connect Under Reset" mode. For more help, refer to the FAQ: "How to Solve Debugger Connection Issues."
Br
2025-06-04 12:37 AM - edited 2025-06-04 12:38 AM
Welcome to the forum.
Please see How to write your question to maximize your chances to find a solution for best results; in particular, please give full details of your development host and target hardware setup.
@ra345j wrote:getting "Error: No STM32 target found!" When trying to connect.
Where, exactly, are you getting that? what tool(s) & versions are you using?
Please show the full logs & messages you get.
@ra345j wrote:I am using an ST-Link V2 with a Tag-connect TC2050-ARM2010 and TC2050-IDC cable
Is it a genuine ST-Link?
How to recognize a genuine ST-LINK/V2 versus a cloned one.
Are you sure the cable wiring is correct?
As @TDK said, please show a schematic.
Some good, clear photos may also help
See also:
How to solve connection errors when connecting and programming the STM32 target board.
How to solve debugger connection issues.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.