STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32N657X0 with Classic USB device middleware

I am trying to add the NUCLEO-N657X0-Q (MB194-N657X0Q-C01) to the IMBootloader project, which currently uses the Legacy Classic USB device middleware. I ran into a problem where, after calling the HAL_PCD_Start() function, I receive an unexpected int...

IgorMisic_0-1749049890954.png
IgorMisic by Associate II
  • 1227 Views
  • 1 replies
  • 0 kudos

Resolved! Can't make Ethernet work for STM32H757I-EVAL

Hello,I followed https://community.st.com/t5/stm32-mcus/how-to-create-a-project-for-stm32h7-with-ethernet-and-lwip-stack/ta-p/49308 tutorial from the scratch to the end, including the Hello UDP part, and adding the "ETH CODE" code.However, I can't pi...

Matteo-uC by Associate III
  • 5632 Views
  • 24 replies
  • 6 kudos

Resolved! STM32H755ZIQ ADC to DMA Failure

Hello! I am trying to trigger an ADC sample to write to DMA via a timer and trigger a green LED on PB0 after every sample so I can use an oscilloscope to verify the sampling speed. However, I believe after trying to debug as best I can, I do not have...

kyleg4032 by Associate II
  • 1327 Views
  • 3 replies
  • 2 kudos

Ethernet +LWIP +FREERTOS on stm32f407 board

Hi all I am trying to run ethernet stack along with freertos using TcpServer,so the issue what I am facing is I am not able to ping my board via hercules. I have checked all the configuration and register MAC MMC DMA is fine and even my three tasks 1...

Ash1 by Associate III
  • 3020 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.