STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H563RGT6 with LAN8742A phy

Hi as part of my project I am trying to integrate the mentioned parts in subject to control modbus eth relay over tcpip.What I have done so far.1. Integrated Lan chip driver to stm32 library and initalization done.2. Integrated LwIP stack from online...

aravindpv_0-1750917437924.png aravindpv_1-1750917664915.png aravindpv_2-1750917679386.png
aravindpv by Associate III
  • 2927 Views
  • 14 replies
  • 3 kudos

Resolved! STM32N6 VENC Power measurement example code

Good day folks!I trust you are well.Do you know where I can find the example that was used to take the VENC power measurements as outlined on this Wiki page ?I can't seem to find it under the Applications and Examples in the STM32CubeN6 v1.2.0 Specif...

exarian_0-1752838699556.png
exarian by Associate III
  • 646 Views
  • 2 replies
  • 0 kudos

Resolved! SPI in STM32F427 in slave mode

Hi, gents,     I have some need to use SPI slave mode instead of working SPI master mode.     I'm tranferring 22 16-bit words from Infineon slave board at 6Mhz clock rate, once per 100 ns, and have 4-line interface including CS line. Due to noisy lin...

DR77 by Associate II
  • 1527 Views
  • 3 replies
  • 0 kudos

STM32N6 VENC at lower resolutions

Hi everyone,I have successfully deployed the VENC_SDCARD example on the board and can see its feed on my laptop. Now, I want to record it at 480x480 resolution instead of the default 800x480 provided in the example.I have modified the buffer size, DC...

Image (1).jpeg Screenshot from 2025-07-15 13-41-14.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.