STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F767 Nucleo: ethernet not working

Posted on July 25, 2016 at 12:18Has anyone got ethernet working on the STM32F767 or similar board? I didn't see any examples for this board, so I used the CubeMX tool to generate the initialization code with ethernet on. Then I adapted the LWIP exam...

STM32F3 ADC problem with HAL library

Posted on January 29, 2017 at 15:52Hi, I'm new to STM32 microcontrollers, now I have STM32F3Discovery board and I want to implement a signal follower.The microcontroller read the signal from ADC1 pin A0 and generate it on DAC1 channel2.when I have c...

0690X00000603TLQAY.jpg

STM32L476 high current draw before programming

Posted on January 06, 2017 at 22:16Our application uses the SMT32L4 in a 4-20mA loop-powered transmitter. VCC on this device is 3V. The typical current draw once the product is operational is approximately 8mA @ 3v. We are utilizing the bootloader t...

gwillette by Associate II
  • 9990 Views
  • 22 replies
  • 0 kudos

STM32L Flash HalfPageProgram problem

Posted on April 18, 2015 at 23:00Hi,I am not able to program the flash of a STM32L151RC using ''half page'' programming.Normal programming (word by word) works fine.I have tried it using the 2 latest GCC compilers (4.8.4), and I have tried with the ...

stm32f767 and UART DMA IT (interrupts)

Posted on January 24, 2017 at 11:07Hi,How to use UART in DMA mode with interrupts IT.I use the next code to transmit, and it works perfect. HAL_DMA_Start_IT(&hdma_usart3_tx, (uint32_t)msg, (uint32_t)&huart3.Instance->TDR, strlen(msg)); huart3.Instan...

embvis by Associate III
  • 2810 Views
  • 5 replies
  • 0 kudos

USB to Ethernet bridge

Posted on January 24, 2017 at 12:53Hello,I want to make a bridge from USB to Ethernet, to give connectivity to a tablet.I am using an STM32F107RC, a DP83848CVV phyter and the CubeMX to generate the code with this configuration:I do not know how to l...

0690X000006067MQAQ.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.