STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to receive variable length I2C messages?

Posted on February 10, 2017 at 07:20Hello, I'm trying to write an I2C slave using HAL which can accept variable length packet sizes.  I know this question has been asked before but haven't seen any solutions yet! The master can send data packets of ...

sasha by Associate III
  • 1578 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F767 - Fail to access uart bootloader

Posted on January 26, 2017 at 15:09Hello,I'm using a STM32F767BI and I want to use the bootloader functonnality. I want to use USART1 (PA9/PA10) and the BOOT0 pin. I read AN2606 and I use pattern 9  (nDBANK(bit) = 1, Boot(pin) = 1 and BOOT_ADD1(opti...

Erase before new Flash write in STM32F0xx

Posted on February 05, 2017 at 14:27Hi.I am working on STM32F072RB MCU. I can able to Program and Erase the Flash Page. But, I have few doubt about Flash programming:). Sometimes the Data is not written in Flash, when i erase a same and write again ...

STM32L432KC HAL_PCDEx_BCD_VBUSDetect Bug

Posted on February 04, 2017 at 04:11I am using CubeMX with the STM32L4 1.5.2 library. [EDIT -- just confirmed that this exists in 1.6.0 as well]The non-OTG implementation of HAL_PCDEx_BCD_VBUSDetect() will only call  HAL_PCDEx_BCD_Callback() with PC...

firmware download from usb

Posted on January 30, 2017 at 17:36Hi,I am using stm32f429 mcu and i can use usb communication with my board. I want to learn how to download my hex file to mcu from usb port of the mcu. In other words i want to use a simple gui software on my compu...

er3481 by Senior
  • 3734 Views
  • 11 replies
  • 0 kudos

STM32Cube/HAL USB CDC - TX Complete Callback?

Posted on December 14, 2016 at 06:10Hi all,Does anyone know of the 'correct' way to get a call back when the previous transfer has been completed?The USB CDC has the TxState status variable which is cleared when a transmission is complete, but i don...

mwp by Senior
  • 4719 Views
  • 3 replies
  • 0 kudos

STM32L4 discovery OTG HOST Problem

Posted on February 01, 2017 at 10:43Hai,   i am using STM32L476 Discovery Board.For USB Device it is working Perfectly. For OTG Host,mass storage class with USB disk FATFS the pen drive is not mounting on the Host STM32.Give me the solution for this...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.