STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB microphone from the USB speaker example

Hi,Tried to convert STM32CubeN6\Projects\STM32N6570-DK\Applications\USBX\Ux_Device_Audio_2.0 example of the USB speaker to the USB microphone on STM32N6570-DK.The USB device is enumerated as an audio recording device, ux_device_class_audio_stream_fra...

ERROR by Senior
  • 475 Views
  • 1 replies
  • 0 kudos

Push Pull PWM

Hello ST, I am having some trouble generating two PWM signals for a push pull converter.  Ideally I would like the PWM outputs to look like this, I would like the PWM frequency to be 100kHz and a duty cycle range of 0% to 50%. I have connected the p...

allanoverst_0-1762377988597.png PWM PA0 and PA1.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.