2024-06-25 10:14 AM
#include <SWOStream.h>
SWOStream s(2000000, SWO_Async, 0, false); //swoEnable = false
void setup() {
delay(150);
}
void loop() {
s.print("Serial is alive!");
delay(500);
}
Solved! Go to Solution.
2024-06-26 11:44 AM
@BarryWhit wrote:That looks just like the cheap chinese ones. I know because I had one and instead of risking damaging it with my shaky hands to get SWV working, I got a better quality one which worked immediately. Are you sure you bought that from ST?
https://www.eevblog.com/forum/microcontrollers/quick-hack-to-get-swo-on-st-link-clones/
I could have sworn I did buy it from ST, but darn, I'll have to make sure. Before I risk damaging it with the bodge wire (haha), is it possible to get SWV working using the SWIM pin?
2024-06-26 12:59 PM - edited 2024-06-26 2:18 PM
The SWO pin isn't routed to the external connector on these clones, AFAIK there's no way around a bodge to get it working.
If you attempt the mod, be very careful. The PCB inside the clone can change from seller to seller and over time. An EEVblog post from 10 years ago might contain information that does not apply to your board so make sure you're not blindly following but actually understand what you're trying to do. Or, buy a better ST-LINK (original or clone).
2024-06-26 1:17 PM
@BarryWhit wrote:The SWO pin isn't routed to the external connector on these clones, AFAIK there's no way around a bodge to get it working.
If you attempt the mode, be very careful. Clones are uncharted territory, and the board may change from seller to seller and over time. An EEVblog post from 10 years ago may contain information that does not apply to your board so make sure you're not blindly following but actually understand what you're trying to to. Or, buy a better ST-LINK (original or clone).
Sigh, that's a good point. I'll just try to order a new one and make sure it's not a clone, thanks for all of your help!
2024-06-30 8:35 AM - edited 2024-06-30 8:36 AM
@vs13 , see this thread for identical situation and high-res photos of mod (may or may not be same board as yours), if you're thinking of doing it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.