2024-12-25 5:10 PM - edited 2024-12-26 5:25 PM
So originally, I was using a custom bootloader and painfully sending 32 bytes over custom HID to my device. It works, but it's really slow. Not related, but I just want you to know how dumb I am...
Anyway,
I followed the tutorial to use DFU USB interface to patch application firmware.
https://www.youtube.com/watch?v=n_LDXOQHerU
I can't get the DFU programmer working on STM32 Cube Programmer because it can't erase properly.
=================== STM32 Cube Programmer Fail ===================
19:29:25 : UR connection mode is defined with the HWrst reset mode
19:29:27 : USB speed : Full Speed (12MBit/s)
19:29:27 : Manuf. ID : Demo LLC
19:29:27 : Product ID : STM32 DownLoad Firmware Update
19:29:27 : SN : 205C32824358
19:29:27 : DFU protocol: 1.1
19:29:27 : Board : --
19:29:27 : IAP
19:29:51 : Memory Programming ...
19:29:51 : Opening and parsing file: Demo_MainFirmware.bin
19:29:51 : File : Demo_MainFirmware.bin
19:29:51 : Size : 69.75 KB
19:29:51 : Address : 0x0800C100
19:29:51 : Erasing memory corresponding to segment 0:
19:29:51 : Error: failed to erase memory
==========================================================
So I used dfu-util tool instead. Which would work the first time as you can see. I would have it successfully jump to the application code, But if i try to do it again, It only erases first few bytes before stopping.
=================== dfu-util Tool Sucess ===================
F:\Demo\Demo_DesktopApp\src\tools\dfu-util\win64>dfu-util.exe -d 0x0483:0x580c -a 0 -s 0x0800C100:leave -D "Demo_MainFirmware.bin"
dfu-util 0.11
Copyright 2005-2009 Weston Schmidt, Harald Welte and OpenMoko Inc.
Copyright 2010-2021 Tormod Volden and Stefan Schmidt
This program is Free Software and has ABSOLUTELY NO WARRANTY
Please report bugs to http://sourceforge.net/p/dfu-util/tickets/
Warning: Invalid DFU suffix signature
A valid DFU suffix will be required in a future dfu-util release
Opening DFU capable USB device...
Device ID 0483:580c
Device DFU version 011a
Claiming USB DFU Interface...
Setting Alternate Interface #0 ...
Determining device status...
DFU state(2) = dfuIDLE, status(0) = No error condition is present
DFU mode device DFU version 011a
Device returned transfer size 1024
DfuSe interface name: "Internal Flash "
Downloading element to address = 0x0800c100, size = 71428
Erase [=========================] 100% 71428 bytes
Erase done.
Download [=========================] 100% 71428 bytes
Download done.
File downloaded successfully
Submitting leave request...
Transitioning to dfuMANIFEST state
==========================================================
Now if I put my device in bootloader mode and send it again, it gets stuck every single time around 4096 bytes
=================== dfu-util Tool Fail ===================
Warning: Invalid DFU suffix signature
A valid DFU suffix will be required in a future dfu-util release
Opening DFU capable USB device...
Device ID 0483:580c
Device DFU version 011a
Claiming USB DFU Interface...
Setting Alternate Interface #0 ...
Determining device status...
DFU state(2) = dfuIDLE, status(0) = No error condition is present
DFU mode device DFU version 011a
Device returned transfer size 1024
DfuSe interface name: "Internal Flash "
Downloading element to address = 0x0800c100, size = 71428
Erase [=========================] 100% 71428 bytes
Erase done.
Download [= ] 4% 3072 bytesError during download get_status
==========================================================
I already set the priority for sys tick to be higher than usb for the interrupt priority. If I was to take a guess what I did wrong, the linker memory isn't aligned properly to erase pages, FLASH_DESC_STR is wrong, or im handling erasing wrong on my Cortex M0 microcontroller.
Also I tried to full send it and set FLASH_DESC_STR to "@Internal Flash /0x08000000/128*1Kg" to see if i can get erase working. Nope the programming tool does not like that lol.
Also #define USBD_DFU_APP_DEFAULT_ADD 0x0800C100
Any wisdom you have helps. I am using a custom STM32F070CBTX board I made, so there isnt any UART for debugging, The USB is being used for the DFU patching, and my SWD doesnt support serial wire viewer. So until I get another board made to see debugging better, im stumped.
Thanks and Happy Holidays!
2025-08-22 5:10 AM
Hi @Lumenski
The issue is more likely related to CubeProgrammer. I am moving the thread to CubeProgrammer forum.
Have you tried performing a full chip erase before upgrading the firmware.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.