Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
I have a 3d printer with a Btt skr pro v1.2 motherboard. The Sd card slot is non functional so looking to update the firmware directly.can I use a st-link v2 to upload the firmware from the pc to the motherboard? the motherboard has a stm32 controlle...
Hi,I'm willing to use the MXCHIP EMW3080B wireless module on the B-U585I-IOT02A in a project with TrustZone enabled. As there is no tutorial for that, I copied files from the Nx_Network_Basics example.Unfortunately I get the following error when buil...
Hi, I'm encountering a general issue with DMA on the STM32H743 processor. I'm having trouble with SPI and I2C communication when using multiple integrated devices. For instance, when attempting SPI DMA communication with the W5500 integrated circuit,...
Please confirm the default state of BOOT1 pin state through nBOOT1 bit for BOOT configuration. How can we pre-configure nBOOT1 bit for BOOT configuration?
Hello everyone, I am a student who is fairly new to these concepts so I wanted to pick your brains for a bit if you'll allow me to. I have done some research and found that STM32F4 is compatible with AT commands if we use external hardware. However, ...
Dear ST, In UM1974 rev 10, section 6.8.1, page 25/84 a recommendation is given for the use of a particular crystal part number: This part number does not exist. I've searched on both Digikey and LCSC and in both there is only the part numberNX3225GD-...
Hello everyone. I am getting started with SPI and am here with what I believe to be a pretty simple mistake or oversight on my part that I am just not seeing. For the first part of this project, I wish to create a file named "write.txt" on my SD card...
Using B-L072Z-LRWAN Board, I'm trying to Enumerate the USB Port as a Ethernet Adapter.(As Device not Host)Thereby I integrated just the USB-ECM Stack provided by the STM32 itself.I initially had issues with Driver, Post Following the Guide/Post from ...
Hi Community,I'm new to working with STM32 microcontrollers and I'm encountering a challenge when transmitting data through SPI on my STM32 Nucleo board. I'd appreciate some guidance from the experienced members of this community.My Goal:Transmit the...
I'm trying to use Arduino 2.3.2 with an STM32F405 board and I configured it to use these recommended settings, but I can't open the Serial monitor for the board. It can connect to my laptop and even upload code successfully, but I can't access the po...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.