2023-02-08 1:41 AM
I've have a custom board with a STM32G031,from the board we have access to the following MCU pins:
I've connected this 4 pins to a ST-LINK/V2. Like this (left) mcu, (right) st-link.
The current delivered by PSU goes to almost 0 after trying to flash (around 0.004A from the correct 0.041A). When trying to flash the uC these are the errors/log I get:
10:37:32 : ST-LINK SN : 55FF6E067871515343241267
10:37:32 : ST-LINK FW : V2J39S7
10:37:32 : Board : --
10:37:32 : Voltage : 2,60V
10:37:32 : SWD freq : 4000 KHz
10:37:32 : Connect mode: Normal
10:37:32 : Reset mode : Software reset
10:37:32 : Device ID : 0x466
10:37:32 : Revision ID : Rev 1.1
10:37:35 : Error: Database: There's no active configuration for this device. All the 6 configurations are disabled!
10:37:35 : Debug in Low Power mode is not supported for this device.
10:37:36 : UPLOADING OPTION BYTES DATA ...
10:37:36 : Bank : 0x00
10:37:36 : Address : 0x40022020
10:37:36 : Size : 108 Bytes
10:37:36 : Error: Uploading Option Bytes bank: 0 failed
10:37:38 : Error: Initializing the Option Bytes failed
10:37:38 : Disconnected from device.Isolating the errors:
Error: Database: There's no active configuration for this device. All the 6 configurations are disabled!
Error: Uploading Option Bytes bank: 0 failed
Error: Initializing the Option Bytes failedAny ideas on how to solve this?
Thanks!
Solved! Go to Solution.
2023-02-17 12:31 AM
I'm getting a very similar problem, new board design with STM32G031G4. Any suggestions welcome!
Using STM32CubeProgrammer and STLink, when I connect I get
Error: Database: There's no active configuration for this device. All the 6 configurations are disabled!and when I program flash I get
File segment @0x08000000 is not 255-bytes aligned. It will be aligned to @0x07FFFFF8If I connect to a NUCLEO-G031K8 instead, it connects and programs just fine, so I'm assuming these errors are due to a problem on the target board, not anything at the PC end. I also tried STM32CubeIDE, same errors. But if I use the old STM32 ST-Link Utility it can program the target just fine. And STM32CubeProgrammer can then verify the target (compare with file), but still cannot program it. So I guess the STM32Cube* apps are doing things differently to the old stlink utility.
Had a good look at signals with a scope, all looks clean, ground and 3V3 clean. Very simple board, standard SWD connections, I've done lots of similar designs with no problems. Tried running ST-Link at minimum speed, same. What seems strange is it connects, and reads Device ID : 0x466 Revision ID : Rev Y, so SWD basics are working.
Here's the log from an attempted connect and program
08:20:14 : ST-LINK SN : 53FF6C067287555144431867
08:20:14 : ST-LINK FW : V2J40S7
08:20:14 : Board : --
08:20:14 : Voltage : 3.23V
08:20:14 : SWD freq : 100 KHz
08:20:14 : Connect mode: Normal
08:20:14 : Reset mode : Hardware reset
08:20:14 : Device ID : 0x466
08:20:14 : Revision ID : Rev Y
08:20:14 : Error: Database: There's no active configuration for this device. All the 6 configurations are disabled!
08:20:14 : UPLOADING OPTION BYTES DATA ...
08:20:14 : Bank : 0x00
08:20:14 : Address : 0x40022020
08:20:14 : Size : 108 Bytes
08:20:14 : Bank : 0x01
08:20:14 : Address : 0x40022080
08:20:14 : Size : 4 Bytes
08:20:14 : UPLOADING ...
08:20:14 : Size : 1024 Bytes
08:20:14 : Address : 0x8000000
08:20:14 : Read progress:
08:20:15 : Data read successfully
08:20:15 : Time elapsed during the read operation is: 00:00:00.660
08:20:54 : Memory Programming ...
08:20:54 : Opening and parsing file: wf3826.elf
08:20:54 : File : wf3826.elf
08:20:54 : Size : 3.45 KB
08:20:54 : Address : 0x08000000
08:20:54 : Erasing memory corresponding to segment 0:
08:20:54 : Erasing external memory sectors [0 1]
08:20:55 : File segment @0x08000000 is not 255-bytes aligned. It will be aligned to @0x07FFFFF8
08:20:55 : Download in Progress:
08:20:55 : Error: failed to download Segment[0]
08:20:55 : Error: failed to download the FileAny suggestions? Thanks
2023-02-17 12:57 AM
Seems your elf linking script error or buggy stmprogrammer sw. Try flash bin file...
2023-02-17 1:39 AM
I've tried a bin file, same error (File segment @0x08000000 is not 255-bytes aligned. It will be aligned to @0x07FFFFF8). And it works fine if I connect to nucleo board instead of target. And that wouldn't explain the "Error: Database: There's no active configuration for this device" error when I connect.
So I'm thinking something else is going wrong and the PC apps are throwing spurious errors.
2023-02-17 2:08 AM
K8 and G4 is different id , but yes maybe other trouble on your board, check vcap power usw...
Somtimes reported errors from prog is long way from real...
2023-02-17 2:12 AM
I've been looking at the Revision ID, STM32Prog reports Rev Y for my board (and Rev 1.1 for NUCLEO). Looking at the reference manual (RM0444 Rev 5) page 1374 Table 254. REV_ID field values, it only lists A (1.0) and Z (1.1). So I'm guessing STM32Prog isn't recognising these Rev Y chips and so is doing silly things. Would explain the "Error: Database: There's no active configuration for this device"
Also, looking at Option Bytes in STM32Prog, it lists lots of duplicates, e.g. BOR_EN, BORF_LEV, BOR_LEV & NRST_MODE each repeated 4 times. Again I guess this could be a symptom of the above.
Why have I got Rev Y chips? And why are they not supported/listed? I guess this a question for ST
2023-02-17 2:41 AM
Just spotted, in Errata ES0487 Rev 5, they added silicon revision Y in May 2022.
Why is it not supported? I'm running latest STM32CubeProgrammer V2.12.0
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.