2026-01-22 8:12 AM - last edited on 2026-02-27 4:01 AM by KDJEM.1
I am using an STM32H755ZQ device and unable to start a debug session using STM32CubeIDE + ST-LINK (SWD).
The system uses two STM32 controllers, where firmware is flashed to one controller and data is shared/communicated to the second controller.
Debug fails with errors like DEV_TARGET_HELD_UNDER_RESET and GDB connection timeout (localhost:61234).
Even with Connect under reset, low SWD frequency, and full chip erase via STM32CubeProgrammer, the issue persists.
Looking for guidance on whether inter-controller communication, reset interaction, or H755-specific debug/security settings could block debugging.
2026-01-23 12:51 AM
Hello @venkatakrishnan and welcome to the ST community.
You need to provide more details about the hardware you are using and what power configuration is set by hardware SMPS, LDO etc..?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.