2026-01-22 8:40 PM
Hello,
I’m working on a project with the NUCLEO-H753ZI board and need to connect multiple devices. I’d like to know:
1. How many GPIO pins are 5 V-tolerant for digital input?
2. How many GPIO pins are available for general use, both 3.3 V-only and 5 V-tolerant, considering the board’s default peripherals?
I want to make sure I safely use the MCU’s GPIOs for my inputs and outputs. Any guidance or reference resources would be appreciated.
Thank You!
2026-01-22 8:58 PM
In DS12117 taken from https://www.st.com/resource/en/datasheet/stm32h753zi.pdf you find a table 8 "Pin/ball definition" (starting on page 64). Pins marked as "FT" are 5V tolerant as given in table 7.
HTH Klaus
2026-01-22 9:06 PM
See also the schematic for the board. Most pins are 5V tolerant.
https://www.st.com/resource/en/schematic_pack/mb1364-h753zi-e01-schematic.pdf
I suggest approaching this the other way--decide how many 5V tolerant pins you need then find a board that supports that. If you need 40-50 or less, you should have no problem.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.