STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

GPIO Pins(Nucleo-H753zi)

Hello,I’m working on a project with the NUCLEO-H753ZI board and need to connect multiple devices. I’d like to know:1. How many GPIO pins are 5 V-tolerant for digital input?2. How many GPIO pins are available for general use, both 3.3 V-only and 5 V-t...

Kishen31 by Associate
  • 266 Views
  • 2 replies
  • 0 kudos

Stlink-V3PWR & OpenOCD

Hello,I want to use the STLink-V3PWR and OpenOCD in SWD mode. I can just use hla_swd as transport and not SWD otherwise I will get the error "Debug adapter doesn't support 'swd' transport". Is there no possibility to use SWD?BR

Resolved! Nucleo-F767ZI must reset after power ON

Hello everyone, my programme on Nucleo-F767ZI do not run when I power ON by external power supply. I force to press reset button or power supply st-link by usb cable.I searched some solutions such as: BOOT0 to GND; or turn on bit POR = 1 in RCC_CSR, ...

ManhPham by Associate III
  • 4225 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.