2026-04-16 5:23 AM - edited 2026-04-16 5:27 AM
Hello,
On a STM32H7RS are using the USB_OTG_HS peripheral in PCD_SPEED_FULL mode using internal clock.
After I was able to configure the clock so that the MCU is responding on enumeration requests. The responses however seem to be partially incorrect; the trace tool shows stalls.
I did not found an example in current https://github.com/STMicroelectronics/STM32CubeH7RS
The following changes are applied to a CubeMX generated project
main.c SystemClock_Config:
LL3.PLLN was set to output 24 MHz
RCC_OscInitStruct.PLL3.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL3.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL3.PLLM = 4;
RCC_OscInitStruct.PLL3.PLLN = 60;
RCC_OscInitStruct.PLL3.PLLP = 2;
RCC_OscInitStruct.PLL3.PLLQ = 40;
RCC_OscInitStruct.PLL3.PLLR = 16;
RCC_OscInitStruct.PLL3.PLLS = 2;
RCC_OscInitStruct.PLL3.PLLT = 2;Configure CRS
__HAL_RCC_CRS_CLK_ENABLE();
RCC_CRSInitTypeDef RCC_CRSInitStruct = {0};
RCC_CRSInitStruct.Prescaler = RCC_CRS_SYNC_DIV1; // default
RCC_CRSInitStruct.Source = RCC_CRS_SYNC_SOURCE_USB_OTG_HS; //RCC_CRS_SYNC_SOURCE_USB_OTG_FS;
RCC_CRSInitStruct.Polarity = RCC_CRS_SYNC_POLARITY_RISING;
RCC_CRSInitStruct.ReloadValue = __HAL_RCC_CRS_RELOADVALUE_CALCULATE(48000000,1000); // RCC_CRS_RELOADVALUE_DEFAULT = 0x0000BB7FU
RCC_CRSInitStruct.ErrorLimitValue = 34; // = RCC_CRS_ERRORLIMIT_DEFAULT
RCC_CRSInitStruct.HSI48CalibrationValue = 32; // = RCC_CRS_HSI48CALIBRATION_DEFAULT
HAL_RCCEx_CRSConfig(&RCC_CRSInitStruct);usbd_conf.c
void HAL_PCD_MspInit(PCD_HandleTypeDef* pcdHandle)
{
RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
if(pcdHandle->Instance==USB_OTG_HS)
{
/* USER CODE BEGIN USB_OTG_FS_MspInit 0 */
/* USER CODE END USB_OTG_FS_MspInit 0 */
/** Initializes the peripherals clock
*/
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USBPHYC;
PeriphClkInit.UsbPhycClockSelection = RCC_USBPHYCCLKSOURCE_PLL3Q;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
{
Error_Handler();
}
/** Enable USB Voltage detector
*/
if(HAL_PWREx_EnableUSBVoltageDetector() != HAL_OK)
Error_Handler();
HAL_PWREx_EnableUSBHSregulator();
/* Peripheral clock enable */
__HAL_RCC_USB_OTG_HS_CLK_ENABLE();
__HAL_RCC_USBPHYC_CLK_ENABLE();
/* Peripheral interrupt init */
HAL_NVIC_SetPriority(OTG_HS_IRQn, 5, 0);
HAL_NVIC_EnableIRQ(OTG_HS_IRQn);
/* USER CODE BEGIN USB_OTG_FS_MspInit 1 */
/* USER CODE END USB_OTG_FS_MspInit 1 */
}
}I checked the following related posts
STM32H7R3 USB FS device enumeration problem | Community
What is missing/wrong in my configuration?
Many thanks for any help.
Solved! Go to Solution.
2026-04-27 9:52 AM
Hi @h p
Based on your code provided,
#if MOD_4 == 600
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI48|RCC_OSCILLATORTYPE_HSI;
HSI48 should not be part of the SYSCLK source setup.
On STM32H7RS, HSI48 is intended as a kernel clock for specific peripherals such as USB and RNG, as described in the reference manual and the CubeMX clock tree. It is not meant to feed the main system clock.
Second, you should use better dividers like
RCC_OscInitStruct.PLL1.PLLM = 8; //instead of 32
RCC_OscInitStruct.PLL1.PLLN = 75; //instead of 300
This would be more consistent with generating a 600 MHz system clock, depending on your input clock source and the rest of the PLL configuration.
Also here, I assume this should be inversed
#if MOD_4 != 0
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
#else
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
#endif
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-04-17 4:01 AM
Hello @h p
Would you attach your example code to reproduce on my end?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-04-23 1:34 AM
Hello @FBL
I created a CubeMX Project and applied necessary patches (MOD_1, MOD2, optionally MOD_3 switches in stm32h7rsxx_hal_conf). It works on the STM32H7S78-DK. The enumeration works successfully. The SYSCLK is 64MHz (MOD_4 set to 0).
When the SYSCLK is switched to 600 MHz using PLLCLK (MOD_4 set to 600) I observe the same problem as on our board: The enumeration fails. Either the trace shows incomplete frames or no activity at all.
The attached project demonstrates the problem. If MOD_4 is set back to 0 then the enumeration is successful.
Best reards,
2026-04-27 9:52 AM
Hi @h p
Based on your code provided,
#if MOD_4 == 600
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI48|RCC_OSCILLATORTYPE_HSI;
HSI48 should not be part of the SYSCLK source setup.
On STM32H7RS, HSI48 is intended as a kernel clock for specific peripherals such as USB and RNG, as described in the reference manual and the CubeMX clock tree. It is not meant to feed the main system clock.
Second, you should use better dividers like
RCC_OscInitStruct.PLL1.PLLM = 8; //instead of 32
RCC_OscInitStruct.PLL1.PLLN = 75; //instead of 300
This would be more consistent with generating a 600 MHz system clock, depending on your input clock source and the rest of the PLL configuration.
Also here, I assume this should be inversed
#if MOD_4 != 0
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
#else
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
#endif
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-05-04 7:13 AM
Hello @FBL
Thanks a lot for your advice. I changed the code accordingly. To make the provided test project work in case 600 MHz is used, the RCC must be configured as follows. This is missing in the provided test project.
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV2;
RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV2;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK)
{
Error_Handler();
} By this USBD FS on OTG FS works with all clock configuration (HSI/HSE) on both the eval board and our HW.
In the original project I had an additional error: I copied the code from MX_USB_DEVICE_Init (USBD_Init/USBD_RegisterClass/USBD_CDC_RegisterInterface and used another name for the USBD_HandleTypeDef instance). I missed that the instance is also used in usbd_cdc_if.c.
Best regards,
@h p
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.