2021-12-21 2:03 AM
Hi,
We are planing to use stm32g4 higher end micro controller 128 pins(107 GPIO). We had faced issue for pin shortage.
We want to know JTAG, Oscillator we can use as multi functionality (Ex - Debug as well as GPIO or etc...) functionality ?
Pins:
PA15 - SYS_JTDI
PA14 - SYS_JTCK-SWCLK
PA13 - SYS_JTMS-SWDIO
PB3 - SYS_JTDO-SWO
G10 - NRST
PF0 - OSC_IN
PF1 - OCC_OUT
PG10 - NRST
PC14 - OSC32_IN
PC15 - OSC32_OUT
PB8 - BOOT0
We not going to use RTC can we use OSC32_IN, OSC32_OUT as GPIO or other peripheral ?
TI has any faster GPIO extender(more pins) recommenced ic's ?
Thanks & Regards,
Vasu
2021-12-21 5:34 AM
If you use ST_LINK for debug (and not JTAG) you can use PA15 as GPIO/alternate
If you don't need SWO (High speed debug trace output) you can use PB3 as GPIO / alternate
You can use RST as GPIO with great care...
If you don't use HSE quartz as system clock source you can usePF0/PF1 as GPIO
If you use HSE bypass as system clock source you can use PF1 as GPIO.
PC14/PC15 can be used as GPIO
PB8 can be used as GPIO. You still provide the right level at boot time or set the internal flash options to ignore the BOOT0 pin (e.g. BOOT_LOCK or nBOOT0 flags). Have a look to RM0440 chapter "Boot configuration" P90.
All is explained in the reference manual RM0440 (Chapter "Boot configuration" P90 for BOOT0 configuration)
2021-12-21 5:37 AM
Note that PC13-PC15 have limited driving capability.
2021-12-21 6:03 AM
I2C IO extenders are very slow...
I use:
For output the well known SN74HC595 for output: 3 command pins, cascadable, > 10MHz clock. Or the faster new SN74HCS595.
For input: SN74HCS165: 3 pins, cascadable, > 40 MHz clock
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.