STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

What are the BOR levels for STM32G030 ?

Hello!When I connect to STM32G030 with the ST-Link programmer in the Options bytes tab, I can adjust the BOR levels (level 1-4 F and R). These levels are not described in the datasheet (DS12991 Rev 3). What are these levels and where can I find their...

Akoli.2 by Associate III
  • 4075 Views
  • 1 replies
  • 0 kudos

Also, I heard "Pull-up resistors are not require because STM32F already have one." is that true? Please help me about it. I will be really appriciated.

 Hi everyone, I am confuse about I2C pull-up resistors. I use 4 I2C sensors. I am not sure is it true that pull-up resistors count. I use every sensors for pull-up resistors. If I use just one I2C port (I mean one port for all sensors) is it enough? 

0693W00000HncMpQAJ.png
AElma.1 by Associate II
  • 8291 Views
  • 5 replies
  • 1 kudos

STM32L073RZT6 hardly booting the firmware

Hello ST Community,I have a PCB designed according to the attached schematic.Recently, I have been struggling with the following awkward issues:1) The flashed firmware (via UART) doest not always start (2/10 attempts lead to successful code execution...

VMeto.1 by Associate II
  • 4195 Views
  • 6 replies
  • 0 kudos

Short circuit on STM32H750

Hello!It's been a while since I'm working with STM32H7 MCUs and now, some of the products using it are returning from my customers, not working at all. Analyzing the board, I get a short circuit between 3V3 and GND and after removing the MCU, the sho...

Peaga by Senior
  • 8880 Views
  • 10 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.