2025-03-18 1:19 AM - last edited on 2025-03-18 2:27 AM by Peter BENSCH
I have this 2 programmers, stlinkv2isol and stlinkv3.
With the first, I'm able to program and debug my board. But with the second, no, I received a message like this
ST-LINK SN : 0050002E3331510633323639
ST-LINK FW : V3J13M4B5S1
Board : STLINK-V3SET
Voltage : 1.78V
Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication
2nd connect tentative with frequency (8MHz)
ST-LINK SN : 0050002E3331510633323639
ST-LINK FW : V3J13M4B5S1
Board : STLINK-V3SET
Voltage : 1.77V
Error: ST-LINK error (DEV_CONNECT_ERR)
Encountered Error when opening C:\ST\STM32CubeIDE_1.16.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.1.400.202404281720\tools\bin\STM32_Programmer_CLI.exe
Error in STM32CubeProgrammer
Shutting down...
Exit.
I'm using the JTAG connector of stlinkv3 (CN2).
Thank you.
Solved! Go to Solution.
2025-03-18 2:26 AM - edited 2025-03-18 2:30 AM
Your target voltage appears to be around 1.8V, which is OK for ST-LINK/V2-ISOL, but no longer for a pure STLINK-V3SET.
Without the B-STLINK-VOLT extension, STLINK-V3SET is intended for a target VCC of 3-3.6V, while ST-LINK/V2-ISOL operates between 1.65-3.6V.
Regards
/Peter
2025-03-18 2:26 AM - edited 2025-03-18 2:30 AM
Your target voltage appears to be around 1.8V, which is OK for ST-LINK/V2-ISOL, but no longer for a pure STLINK-V3SET.
Without the B-STLINK-VOLT extension, STLINK-V3SET is intended for a target VCC of 3-3.6V, while ST-LINK/V2-ISOL operates between 1.65-3.6V.
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.