2015-05-17 3:48 AM
Hi,
I have a STM32F4-Discovery and the ST-Link V2 is not detect on my Dell Latitude 3540, I tried all usb ports, when I plug the usb connector windows not detect nothing. I tried on another PC and is working without problems. On my notebook many another usb periphericals is working without problem. Suggestions? Thank you Giovanni #stlink2015-05-17 7:11 AM
Different versions of Windows? Which?
Different USB ports? All? Shows up in Device Manager? Or Not?2015-05-20 4:44 AM
The problem is not OS I tried Windows 7 and Linux.
My notebook has 4 USB ports: 2 USB3.0 and 2USB2.0 and in all ports there is the problem, I tried also with HUB. In linux in dmesg not appear nothing also errors, in Windows nothing in Device Manager and I don't receive also the sound notification, it's invisible. If
it did not work
on another PCI would have said
is broken. I tried 5 USB cables without success. Thank you GiovanniWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.