Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Posted on June 08, 2015 at 16:33Hello,I've been using STM32 for quite some time. In work I use full ST-Link v2 isol but, in home as hobbys (and soon startuper) I use stlink on stm32f4 disovery board. I had no problems with it untill today. When my e...
Posted on May 25, 2015 at 02:16Hi, I'm using an STM32F302R8 board to do some basic DSP work. I've been using my desktop with windows 7 on it for a while and I'm able to use Keil V5.14 to program the board no problem. However, I have to move to using...
Posted on May 17, 2015 at 12:48Hi, I have a STM32F4-Discovery and the ST-Link V2 is not detect on my Dell Latitude 3540, I tried all usb ports, when I plug the usb connector windows not detect nothing. I tried on another PC and is working without pr...
Posted on May 05, 2015 at 08:09Hi to all, i need to develop my board with ST-link/v2, i want use SWD connector present on board, but the manual is not clear and i don't understand nothing, do you have experience? can you help me? #nucleo #st-link...
Posted on April 29, 2015 at 01:37Hello and thanks for checking this post out. It's my first post, and I am rather lost. I have a STM32L100RB MCU that I am trying to set up a I2C Slave up on. I am interfacing with the MCU via the ST-Link/V1 set up f...
Posted on April 14, 2015 at 01:16I have an application with a F407 that has a correctly working M29W128 that happens to be on NE1 (so the starting address is 0x60000000). The application works wonderfully using a resident bootloader that accepts a ...
Posted on April 15, 2015 at 21:14Hello, I need to program an STM8AF5289TC using an ICT Tester / Fixture and I just saw that ST-LINK/V2 Works just fine and is small and not expensive for integration, but the problem is that PC controller is Windows 2...
Posted on April 15, 2015 at 19:50Hi to all, I'm trying to program my iNemo based custom board with the ST LINK provided with the STM32F4 Discovery. When I try to connect with STM32 ST-Link Utility I get the error: '' Core is held in reset''. Another...
Posted on March 31, 2015 at 13:21Hello! I have strange error while attempting to connect ST-LIK Utility to MCU. Trace log: W at 0xe000edf0: 0xa05f0000 cErrLog::SetLogTraceOn STLinkUSBDriver.dll loaded ST-Link/V2 device detected Target voltage detec...
Posted on March 26, 2015 at 06:25Hi, I'm using IAR EWARM 7.3. I'm using ST-Link, newest firmware. The target is connected via JTAG. It flashes and seems to run OK - the IWDG is ticking fine without crashing, with RTOS running. I can print using ITM_...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.