2025-11-21 10:02 PM
Hello,
I am currently wor
king on connecting an MT9M001 camera module to the STM32F429I-Discovery board and displaying the captured image on a PC.
During this process, I am testing PWM output on the board, but I am experiencing an issue where the output voltage does not swing between 0 V and 3.3 V as expected.
Environment
Board: STM32F429I-Discovery
IDE / Firmware: STM32CubeIDE + HAL (STM32CubeF4 package)
Pin used: PB0 / TIM3_CH3 (Alternate Function, Push-Pull, no pull-up/down)
PWM: Generated with TIM3 (frequency and duty cycle shown in attached code/images)
Measurement: Oscilloscope (×10 probe, GND connected to board GND)
Issue
The PWM waveform output from PB0 shows the following problems:
The low level does not go down to 0 V
The high level does not reach 3.3 V
Before switching to PB0, I was using PA8 (TIM1_CH1), but I observed the same issue—
the voltage could not drop to 0 V.
I received advice that PA8 might be loaded by other on-board circuitry,
so I moved the PWM output to PB0 (TIM3_CH3).
However, the same reduced voltage swing occurs on PB0 as well.
If anyone knows possible causes or has experienced a similar issue,
I would appreciate any guidance.
Solved! Go to Solution.
2025-12-02 1:32 AM
@chachamaru wrote:How can I get a clean 20–24 MHz PWM (XCLK) on this board?
You said in this post that you understood why not:
@chachamaru wrote:I now see that with a 100 MHz scope, only the 3rd harmonic of a 22 MHz square wave is fully visible and the higher harmonics are suppressed.
Therefore, the waveform I am seeing is consistent with the scope and probe limitations.
2025-12-02 1:41 AM
I'm sorry, I didn’t explain it well.
What I meant is this:
If the PWM (XCLK) were being generated correctly, then VSYNC and HSYNC should also be generated correctly by the MT9M001.
So my goal is not to see a perfect waveform on the oscilloscope, but to provide a clean and reliable clock signal into the camera.
Therefore, I want to know how to output a “clear enough” PWM for the microcontroller-to-camera connection, not necessarily a perfect oscilloscope waveform.
2025-12-02 1:44 AM
I suspect that VSYNC and HSYNC are not being generated because the PWM clock signal is not sufficient for the camera.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.