2021-09-11 3:20 PM
On the STM32G431x6/x8/xB UFQFPN48 I've been assuming that BOOT0 pin PB8 was a weak pull-up during reset, but in trying to track this I think it has no pull-ups/ pull-downs. Is this the case?
Solved! Go to Solution.
2021-09-11 5:50 PM
You can use the nBOOT0 option byte to override the value on the pin. Otherwise, you need to ensure it's low or high, depending on your intention.
It should be low if you want to run user code. Whether you do that with a pulldown resistor or an FPGA pin is fine. However, you need to ensure it's low when the STM32 is booting up. The best way to ensure this is an external resistor on the line.
Pulling it up will run the bootloader on startup, rather than user code.
Leaving it floating leads to undefined behavior (unless overridden with option byte mentioned above).
2021-09-11 4:26 PM
Floats, if you use it for BOOT0, pull it low externally to ensure reliable operation. Only the JTAG/SWD pins have pull up/down at power on
2021-09-11 5:46 PM
Presently we use an FPGA open drain output to pull it low. It does not need a pull-up? A float is okay? Thanks!
2021-09-11 5:50 PM
You can use the nBOOT0 option byte to override the value on the pin. Otherwise, you need to ensure it's low or high, depending on your intention.
It should be low if you want to run user code. Whether you do that with a pulldown resistor or an FPGA pin is fine. However, you need to ensure it's low when the STM32 is booting up. The best way to ensure this is an external resistor on the line.
Pulling it up will run the bootloader on startup, rather than user code.
Leaving it floating leads to undefined behavior (unless overridden with option byte mentioned above).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.